Part Number: TAS5828M Other Parts Discussed in Thread: SRC4192 I have a question about the TAS5828M sample rate converter performance. The data sheet does not provide too many details regarding sample rate converter performance.
I have an application…
Part Number: SRC4193 Other Parts Discussed in Thread: SRC4192 , Hi,
Could you please let me know any differences and any time constraints required between the the hard mute by using pin 14 and the soft mute via SPI port? Additionally, is the hard mute function…
Part Number: SRC4193 Other Parts Discussed in Thread: SRC4192 , Does SRC419x support I2S 16bit input data format? I saw the same question but the answer repeated its pdf that has not clear description for I2S mode. So I need just the simple answer yes or…
Other Parts Discussed in Thread: SRC4192 , SRC4190 , SRC4382 Hi Ti members
Purpose : "I2S to SPDIF" Solution
Test equipment -> Audio Precision AP2700 (AP)
Test condition :
AP generate 1K sine wave 0dB to EUT ---> EUT throught the " I2S to SPIF…
Part Number: SRC4192 When the device comes out of reset and there is no CLK (RCKI) present will the device property configure it self based on the control pins being pulled low and high, and then operate properly when RCKI and I2S data is present?
Th…
Part Number: SRC4192 Other Parts Discussed in Thread: PCM5142
I am connecting the SRC4192 to the CS8416 and the PCM5142 with the intention of upsampling 16 bit 48kHz to 24 bit 96 kHz. Both chips are in hardware mode. I have created my schematic based…
Part Number: SRC4192 Hi,
I need to convert a 3 wire I2S input with possible sample rates of 44.1kS/s or 48/96/192 kS/s into a 4 wire I2S at a fixed sample rate (e.g. 48 ks/s) with added master clock (e.g. 24.576 MHz from a local oscillator). According…