Part Number: SRC4193 Hi,
Could you please let me know if there are any disadvantages when LGRP is set to "1" (low group delay)? For example, SNR, distortion, sound quality, etc.
Best regards, Kato
Part Number: SRC4193 Tool/software: Hello everyone. In my setup, the SRC4193 gets a 44.1kHz I2S input with 16 bits on a 32-bit word as a slave. The output is 96kHz and 24 bits on a 32 bit word, also as a slave. The problem I have is that with an input…
Part Number: SRC4193 Other Parts Discussed in Thread: SRC4192 , Hi,
Could you please let me know any differences and any time constraints required between the the hard mute by using pin 14 and the soft mute via SPI port? Additionally, is the hard mute…
Part Number: SRC4193 Hi Team,
Could you help to confirm if SRC4193 support I2C control? We notice I2C is mentioned in 8.2.1 section, but we don't know which pin are assigned to I2C, also don't know the I2C slave address. Please help to confirm, thanks…
Hi Carl,
SRC419x input port can handle audio data word length be up to 24-bits for I2S and Left-Justified formats , while the Right-Justified format supports 16-, 18-, 20-, or 24-bit data . For SRC4193, the data format selection for input port can be…
Part Number: SRC4193 Other Parts Discussed in Thread: SRC4192 , Does SRC419x support I2S 16bit input data format? I saw the same question but the answer repeated its pdf that has not clear description for I2S mode. So I need just the simple answer yes…
Part Number: SRC4193 Hi,
I am considering using one of the SRC419x devices, it will have variable bit depth and sampling rates in but I want the output locked to 16bit 44.1KHz, is it possible to detect when the input is the same as the locked output…
Hi Leonid,
Based on the feedback from design team, the volume control uses 28 bits including the sign bit. Since it is always positive, the effective bits are 27.
Best regards,
Ravi