Part Number: SRC4194 Other Parts Discussed in Thread: TLV320AIC3268 Hi,
My specific design constraint is to convert TDM (TDM8 or 8* TDM4 channels ) into 4 * I2S lines. As I can see in the SRC4194 datasheet, it seems possible to convert I2S to TDM, thanks…
Part Number: SRC4194 Other Parts Discussed in Thread: DIT4192 , Do we have any application notes on how to drive the master clock pin of the SRC4197?
Do you have a check list that would help to make sure that the proper clocks were chosen?
There really…
Other Parts Discussed in Thread: SRC4194 Hi,
Could you please tell us whether we can obtain each audio output as the synchronous output by setting the registers of SCR4194 if the audio sources of the different sampling rates are input to SRC4194 and are…
Other Parts Discussed in Thread: SRC4194 Hi,
I'm using the SRC4194 in software mode, but am unsure whether the unused hardware mode select pins should simply be left floating or tied to GND or VDD?
Many Thanks,
Mark
TSL Products Ltd.
Hi,
If they do not need ADC/DAC and just looking for interface devices then possible option:
2 pieces of SRC4382 or SRC4392: These devices integrate only 2 Channel SRC’s and S/PDIF so we will need two of them.
SRC4184/SRC4194 + DIX9211/DIX4192 …
Part Number: PCM6260-Q1 Other Parts Discussed in Thread: PCM3168A , TLV320AIC3268 , SRC4194 Hi team,
I am looking for replacement for competitor AKM devices as below, could you help to share some advice? Doesn't have to pin to pin, could be functional compatiable…
Hello Kuramochi-san,
Yes, the SRC4184 and SRC4194 are functionally equivalent except the specifications are better (144 vs 128dB) for the SRC4194.
When the output ports are configured in Master mode then they will continue to clock out information even…
Part Number: SRC4194EVM Other Parts Discussed in Thread: SRC4194 I'm trying to use the SRC4194 eval kit in a mode where the SRC chip is acting as a slave on both the input and the output. I'm only using the port A, and the B port is unused.
I…