Part Number: SRC4382 Other Parts Discussed in Thread: DIT4192 Hi Team,
I had a problem configuring DIT with SRC4382 and it never worked.
First application: I2S->PortA-> (optional SRC)->DIT Second application: DIR->SRC->PortA
I'm now debugging…
Part Number: SRC4382 Other Parts Discussed in Thread: DIX4192 , SRC4392 , , SRC4190 Hello,
Do we have a p2p alternative to the CS8422 from Cirrus Logic? It is EOL.
Best regards,
Ambroise
Part Number: SRC4382 Other Parts Discussed in Thread: SRC4392 , during system startup, all registers can be initialized without problem in our application; but we need to change some of register's value such as 0x0D to switch between RX1 and RX2 and are…
Part Number: SRC4382 Other Parts Discussed in Thread: SRC4392
I've a strange issue on writing SRC4382 registers via I2C.
To configure the registers I'm using the i2c-tools application. The first write is to the Page selection register 0x7f 0x00…
Part Number: SRC4382 Hello team,
I've a question on the behaviour of the SRC block RDy pin.
In my application the portA is slave and used to receive an I2S signal that can be present or not (not present means no BCLK, no LRCLK), DIR ch0 is also used…
Zak Kaye said: I appreciate the detail you have provided.
I'm thanking you for the support you are giving.
Zak Kaye said: I have a question about your sequence though, you mention you reload the internal PLL registers and then reset the device?
The…
Part Number: SRC4382 Dear Specialists,
My customer is designing SRC4382 and has a question about unused pins treatment .
I would be grateful if you could advise.
---
Could you please let us know unused pins configuration.
Regarding LOCK, RXCKO, SYNC,…
Part Number: SRC4382 I have 8 instances of the SRC4382.
The measured phase difference of the TX output pins (at the XLR end) between the 8 instances is mostly zero which is what I expect as the MCLK, LRCLK and BCK is the same for the 8 ICs. And the register…
Part Number: SRC4382
Hi Team,
My customer designed the schematic following to the below figure from datasheet. However, it was found that the sampling rate of 192k Hz was not decoded. But if 0.1uF capacitor of TR- was changed to 1uF, it can be decoded…