Part Number: SRC4392EVM-PDK Other Parts Discussed in Thread: SRC4392 , SRC4192 Hi,
I am currently evaluating the SRC4392 module using its development-board.
Is the software necessary in order to test simple TOSLINK input to TOSLINK output configuration…
Part Number: SRC4392 Does the DIR output provide the full 20KHz to 192 KHz sample rate range without having to change any registers? My system seems to need to change the PLL2 output frequency divide by number to produce the correct LR clock once I go…
Part Number: SRC4392 Hi TI,
I'm working on a design which might use the SRC4392 as SPDIF receiver to SRC to I2S slave.
What I need is totally automatic SPDIF receiving and sample rate converting independent of SPDIF sampling rate.
Right now we use…
Part Number: SRC4392 Hello,
I have an application where I need to provide 48KHz Sync Clock and 3.072MHz Bit Clock at all times, can the src4392 do this regardless of what of the recovered clock and Fs values are from the DIR? The case would be: user…
Part Number: SRC4392 Hi,
I'm using SRC4392 at I2C mode.
I follow register to send command, It's work, but I want to check the init sequence, avoid another issue.
Can you support some SRC4392 example code?
Thanks!
Folks,
I guess we can close this thread.
I have a workaround in that I'm sending 24- or 32-bit data, but I would love to understand if the SRC4392 is SUPPOSED to be able to take 16-bit I2S into one Port, pass it through the SRC and output 24-bit I2S from…
Part Number: SRC4392 Other Parts Discussed in Thread: MSP430FR5849 Hi,
I am working on a design using two SRC4392 devices in an audio tester device.
In order to test the host MCU software controlling the SRC4392 devices I am using a SRC4392EVM.
Communication…
Part Number: SRC4392 Dear sirs,
I have SRC4392 configured as follows:
- spdif input signal 96kHz
- DIR routed to PORTA
- PORTA 24 bit, 96 kHz
- MCLK 24.576 MHz
- BCK and LRCLK as output from PORTA
Checked PORTA output signal with scope:
- LRCLCK ok …
Part Number: SRC4392 On very rare occasions, the SRC4392 will keep the SDA line low for no reason and the I2C bus is stuck. I do 2 transactions on the I2C bus every 500ms and after either a few hours up to a full day, the SRC4392 will do this problem…
Dear Steve, same on my side: "You don't have permission to access " e2e.ti.com/.../conversation on this server."
I have 6 x SRC4392 for you
>would you accept my request?
I have try to switch to "accept" - can you try again?…