Part Number: SRC4392EVM-PDK Other Parts Discussed in Thread: SRC4392 Hi Team,
We have a customer that is asking what are the download links needed for this EVM in replacement of the CD.
Thanks!
Part Number: SRC4392EVM-PDK Other Parts Discussed in Thread: SRC4392 Hi there TI guys and girls.
I just received my SRC4392 evaluation module and came to the conclusion that it isn’t shipped with CD-ROMs anymore.
Aver spending many hours on E2E…
Part Number: SRC4392EVM-PDK Other Parts Discussed in Thread: SRC4392 , TLV320AIC3254 Good Morning there,
One of our customer's has received your part # SRC4392EVM-PDK from us, MOUSER ELECTRONICS .
Unfortunately, there was no CD-ROM included in the…
Part Number: SRC4392EVM-PDK Other Parts Discussed in Thread: SRC4392 , Hello
I,m proving the interface SPI of the SRC4392EVM-PDK through the header J22. The signals are provided by a DSP but the SRC4392 doesn´t work.
It receive the signals but there…
Part Number: SRC4392EVM-PDK Good morning
I have started to prove the src4392EVM-PDK with simples instructions. Then I try to read what I have written. However I see that bits are all zeros. Why this is happened?
For example:
Thanks and Regards
Alberto…
Part Number: SRC4392EVM-PDK Other Parts Discussed in Thread: TLV320AIC3254 Good Morning
I'm testing the SRC4392EVM-PDK with the TLV320AIC3254EVM software.
The board is configured for the I2C interfaz. I've introduced two simple commands:
i i2…
Other Parts Discussed in Thread: SRC4392EVM-PDK I recently purchased a SRC4392EVM-PDK and trying to get it work under Windows 7. The CD contains the USB-Serial Commander program and NI-VISA software. Both installs fine. When I connect the PDK, its gets detected…
Hi Steve-san,
Thank you for your explanation.
I am looking forward to getting the root cause and workaround on this issue soon. By the way, could you please tell me how to verify SRC4392EVM-PDK using the external I2S source ?
Best regards, Kato
Hello, Ravi-san,
Our customer wants to compare his measured EVM data in peak value with TI specified rpm value. I show our customer's measurement peak jitter values below.
Condition: SRC OFF Signal Route: RX1 -> DIR -> DIT -> TX Register…
Other Parts Discussed in Thread: SRC4392 , SRC4192 , SRC4392EVM-PDK Hi,
What will hapens, when I apply a signal with sample rate 44,1 kHz from S/PDIF into the SRC4392? SRC4392 is configured for upsampling to 192 kHz and the MCLK is 24,576 MHz . Thanks…