Part Number: STARTERWARE-SITARA Tool/software: TI-RTOS I am working on a project that was sent to me.
I am working in Windows 7. I first imported the project into CCS 8.
The project included pdk_am335x_1_0_5. The project had many includes pointing to this…
Part Number: STARTERWARE-SITARA Other Parts Discussed in Thread: AM5728
Hi, I want the starterware for the IDK-AM5728. In case of IDK-4377, got it inside the TI-sysbios SDK. But when istalled the same for am5728 starterware directory was not present. Objective…
Part Number: STARTERWARE-SITARA Tool/software: Code Composer Studio I'm trying to build the uartEcho project from C:\ti\AM335X_StarterWare_02_00_01_01\build\armv7a\cgt_ccs\am335x\evmAM335x\uart directory and I'm receiving a build error when the program…
Part Number: STARTERWARE-SITARA Other Parts Discussed in Thread: SYSBIOS
Tool/software: TI-RTOS
I am trying to use functions from Starterware 2.0.1.1 with SysBios.
This pages says: "Hence, when the examples are integrated into an RTOS environment, these…
Part Number: STARTERWARE-SITARA
I am using starterware C files with AM335x EVM board to communicate via UART4. We need to use 2 different UART.
We decided to use UART4 as profile 2 is only profile which is supporting CAN and 2 different UART.
We first…
Part Number: STARTERWARE-SITARA I am using AM335x EVM board to communicate with PC using UART4 at 921600 baud rate.
I am using UART4 with FIFO with interrupt mode. Trigger level of FIFO is set to 1.
I have used starterware uartEcho example as base and…
Part Number: STARTERWARE-SITARA Tool/software: Starterware Hey everyone,
i 'm facing some trouble trying to use the eqep module of my beaglebone white. My goal is to print how much the encoder has rotated.
Following is a part of my code which builds…
Part Number: STARTERWARE-SITARA
Trying out the timer examples from StarterWare and pdk version 1.0.7, but cannot find the definitions of APIs declared in uartStdio.h, interrupt.h and evmAM335x.h
Please help with definitions or low level codes of all…
Part Number: STARTERWARE-SITARA
Hello,
Platform Development Kit includes a bootloader project within the starterware directory and the source files contain some PLL settings referenced to the OPP table.
I use SitaraAM3357. The datasheet contain a chapter…
Part Number: STARTERWARE-SITARA
Tool/software: TI-RTOS
Hi, I am using 4377-IDK board. Want to copy u-boot to flash through Jtag. In TI-RTOS starterware,find one qspi flash read/write app,compiled it using CCS. When the loading the same binary through jtag…