Part Number: TPS54331 Dear All,
We Used the SwitcherPro Desktop design tool to design a buck converter with below Spec:
Input volt min = 3.8 v Input volt Max = 5 v
Output volt = 3.1 v Iout Max = 1A
we toke the generated Schematic and complete…
Part Number: TPS40055
Hello,
I've spent the last five months designing and creating the attached SwitcherPro Design schematic using the TPS40055. After many weeks of debugging, I've found that your generated design has some faults. I'm hoping someone…
HI Madhu,
SwitcherPro tool is not supported anymore. This device is also available in WEBENCH and should be the tool used for analyzing and designing with this device. Please give it a try and let us know if you have any questions about it.
Other Parts Discussed in Thread: TPS65400 Hi All,
I know the TPS65400 was added recently to Webench, is it planned to be added to SwitcherPro, which is much more "playable" ?
If not present, is there any other (mono) buck in SwitcherPro which has…
I am sorry you are running into issues using WEBENCH tools. Can you please let us know what issue(s) are running into? If you are looking for a particular feature that you are missing, please let us know about that as well. SwitcherPro Desktop version…
Part Number: TPS40200 SwitcherPro V3.17 calculates very different values for L and C than the Datasheet example P35
Vin: 18V to 52V, Vout=16V @ 1A
L1=100uH, C2 = 22uF
Datasheet P35 Example:
L1 = 220uH, C9 = 330uF
I apologize for replying to a stale discussion - I am looking for gain margin and phase margin on a TPS63000 buck-boost converter. WEBENCH has no phase or gain margin reported for any conditions that I have tried and has no SIM-Bode option. SwitcherPro…
Kohei-san,
Sorry for the delayed response. The discrepancy has been fixed already. Please let me know if you have any questions regarding this.
Regards,
Amod
Yes switcherpro is pretty much legacy software now. It has not had any updates in a few years now, and will not have any in the future. I also still use it occasionally. I have requested many times that webench include some of the functionality that is…
Other Parts Discussed in Thread: TPS61087 , TPS61088 HI, we would like to use SwitherPro to design a 3.6V->6V booster. We had previously done so with TPS61087 and it gave us great results. Unfortunately TPS61088 is missing from the database.
Is there…