Other Parts Discussed in Thread: TPS54528 Hi mates,
When I ran TPS54528 swticherpro simulation, it got some problems about the bode plot.
Spec: Vin=12V, Vout=3.3V, Iout,max=4A
Schematic
Is it the right result?
If yes, why bode plot can not…
I would like to transfer designs from the desktop version of SwitcherPro to the online version. I need to uninstall the desktop version in the near future and wish to preserve my design files for future reference.
Is it possible to use SwitcherPro for TPS2375x PoE designs? I realize that these chips are not included in the bundled libraries, but is there a similar chip to the DC/DC side that can be used to "what if?" the design of a power supply?
Other Parts Discussed in Thread: TPS5401 , TPS54040 In SwitcherPro Desktop Version 3.11.5.2, the program will produce the following error for TPS5401: "The designer could not successfully build a warning-free design with this device and these inputs.…
When I run the SwitcherPro software after I register and down load it, it said: error setting animation value: 0 is not a valid value for Int32. Could you help, Thanks, Thanh Ngo
Other Parts Discussed in Thread: TPS62510 , TPS62065 Hello,
I'm designing a power sensitive application. One of the power topology I'm considering relies on several TPS62510. Is it possible to add this part in switcherpro or to have a way to compute…
Other Parts Discussed in Thread: TPS54060 We've designed +15VDC and -15VDC power supplies using the TPS54060 device.
Now, we'd like to make the designs programmable to be able to adjust the outputs from 7VDC to 15VDC by just varying one resistor in…
Other Parts Discussed in Thread: TPS40210 , LM5022 I have been trying to use switcher pro to design with the TPS40210. I believe my requirements are within the capability of this part, but switcher pro just gives various errors for my inputs.
I…
Hi,
Thanks for your interest for TPS61202. This part does not have either SwitcherPro or WEBENCH model.
Please check our list of all WEBENCH models at:
http://webench.ti.com/webench5/devices/
There is a long list of boost converter models.
Best…