Hi Gerd,
I discussed this issue with some of the C2000 experts. They were able to point me to the correct document for C2000:
/cfs-file/__key/communityserver-discussions-components-files/171/SPRU151A.pdf
However your issue of why you are unable…
Hi,
I installed v9.60.3 on my PC. And find this .dll file.
Please use it and try if it can work on your side. Change the .txt to .dll on your side.
armxds.txt
Best regards,
Cash Hao
J721E_registers2.pdf
hello Sarabesh
The attachment is the register manual. Specific chapter: 7 ENCODER Registers.
Which registers indicate the working status of buf and encoder?
Is the VIDIOC_QUERYBUF command used to query the status of buf? …
Hi Rich,
We typically include the LM95233 temp sensor on our boards, see pg 4 of the schematic.
ADC12D1X00RF_RB-SCH_B.pdf
As far as characterization of the diode, we have some data that we've posted on the forums previously:
This was for the ADC10D1000…
Part Number: AM623 Hi, TI expert!
I have a development environment for am6234, with our own evaluation board.
The software SDK version is PROCESSOR-SDK-LINUX-RT-AM62X-08.06.00.42.
I encountered the following error during multiple system reboots…
Hi,
Thank you for the suggestion. As requested, I disabled the GPU module (pvrsrvkm) and relaunched Weston using CPU-based rendering (Pixman) to isolate whether the issue is related to the GPU or DSS. Below, I'll detail the steps I followed, the configurations…
Hi Krishna,
Here is another forum thread on the topic. http://e2e.ti.com/support/embedded/tirtos/f/355/p/201333/726357.aspx#726357
The capability you are looking for is described in Linux dlopen() and dlsym() (see http://tldp.org/HOWTO/Program-Library…
INGI MIK
INGI MIK said: Question: What is the reason for the PG activating at -5% instead of the datasheet's specified -10% Undervoltage threshold, and what modifications are needed to adjust it to -12%?
The reason PGOOD is responding to less…
Hello Yanko,
Sorry for the inconvenience. The logcat file which I've updated earlier had some build issues because of which CameraHal was not loaded.
Now I've resolved the issue. The CameraHal is now being loaded but still the camera is not working…
Would also recommend section 4.3 of this document. Describes the same HA application (albeit for a ZAP-ZNP operational model). This document is available from the MSP430-ZAP-1.0.3 installer from www.ti.com/z-stack
swrc173.zip (57.0MB) - contains ZStack…