Part Number: TAA5242 Other Parts Discussed in Thread: TAD5242 Hi everybody,
just a short simple question: what's the polarity of the GPO pin (indicating a clock error) at tht TAA5242?
Assumption: Active Hi
Thanks and best regards,
Rainer
Part Number: TAA5242 Other Parts Discussed in Thread: TAD5242 Hi everybody,
I am using a combination of TAA5242 and TAD5242 in TDM4 target mode and supply BCK and FS from a processor.
The GPO of both units is raised and I can't get a reasonable signal…
Part Number: TAA5242 Hi team,
Background: We are evaluating the TAA5242 in Controller I2S mode with an external CCLK (24.576 MHz / 22.5792 MHz). We would like to confirm detailed behavior not fully clear from the datasheet.
Questions:
For MD2…
Part Number: TAA5242 Hi Experts,
The data sheet of TAA5242, in Table 6-9, when MD1/MD2 is configured as high/high, how to configure it to a 48K sampling rate? Is CCLK still required?
In the controller's I2S mode, the default cutoff frequency of the…
Part Number: TAA5242 Hello,
Our customer has a question about power down to power reboot wait time definition described in TAA5242 datasheet "7.3 Power Supply Recommendations".
Would it be possible to suggest whether "at least 100ms" wait time is…
Part Number: TAA5242 Other Parts Discussed in Thread: PCM9211 Hi team,
Is it correct to understand that when operated in single-ended mode, the SNR is reduced by 6 dB from the value stated in the datasheet? Also, does the SNR change with the sampling…
Part Number: TAA5242 Tool/software: Good morning What is the way to connect the I2S signals of two TAA5242 chips in TDM4 master (controller mode).
I can't find the schematic in the data sheet, there is only Fig6.2 for target mode.
My guess is that…
Part Number: TAA5242 Hello,
Our customer has some questions to make sure if his understanding is correct.
1) MD6 pin function ; Is this pin assigned daisy chain input for TDM only, but not assigned for I2S even it looks like TDM only.
2) Does this…
Part Number: TAA5242 Tool/software: Hello,
Our customer needs to know MICBIAS and VREF PSRR performance in 1.8VAVDD. Could you please show us these PSRR reference data if you have.
Best regards,
Part Number: TAA5242 Tool/software: Hello,
Our customer has a simple question about digital IO VIH, VIL specification. He mentioned that VIH, VIL definition is slightly different from IOVDD=1.8V and IOVDD=3.3V condition., that means VIH is defined fixed…