Part Number: TAC5142 Hi,
I would like to ask if there is a Linux driver available for TAC5142.
I know there is such a driver for other members of this family, specifically the ICs which are controlled through I2C (TAC5x1x, www.ti.com/.../1.0) , but…
Part Number: TAC5142 Hello,
Will the codec function correctly if provided with BCLK and FSYNC frequencies that are not exactly the quantities listed in the datasheet, but still achieve a supported ratio?
In our application, we are using an FPGA to…
Part Number: TAC5142 Hi Experts,
I need help confirming the design below.
Im working on a project where I want to process FM radio audio digitally and mix it with other digital audio sources. To do this, I'm using an Si4703 (FM radio IC) and a TAC5142…
Part Number: TAC5142 Other Parts Discussed in Thread: TAC5211 , TAC5111 Tool/software: Is the data format of this device PCM? Or is it some other data format?
(Which data format does it support?)
Because it's not mentioned in the datasheet.
Part Number: TAC5142 Tool/software: Hi team,
I was evaluating the DAC for the TAC5142 and could not confirm the values as per the specs. The following results were obtained
Rated output
2.138Vrms
Minimum Distortion Ratio
0.0055%
…
Part Number: TAC5142 For the TAC5142, we believe that the internal PLL will automatically generate the internal clock from the combination of fsync and BCLK, as described in "without host programming". Is that correct?
In the controller mode of operation…
Part Number: TAC5142EVM-K Other Parts Discussed in Thread: TAC5142 Hello,
when I connect my TAC5142EVM to my PC, it's not detected as audio device since the driver is missing. If I got it correctly, PPC3 is not needed for this EVM since the TAC5142…