Part Number: TAC5212 Other Parts Discussed in Thread: OPA2189 Tool/software: Hi
I want to use TAC5212 in avionics. I have a mono mic so i am using OPA2189 as single ended to differential amplifier. The head phones are also mono so i use OPA2189 as…
Part Number: TAC5212 Other Parts Discussed in Thread: TPS7A20 , TPS631013 Stetho.pdf
we are to use two Analog MEMs microphones in out device. One mic will be a chest piece and the other is environmental sound capture. We would like to substract the…
Part Number: TAC5212 Hi ti team,
The wireless microphone uses the TAC5212 chip, and we are currently encountering the following issue: Does the TAC5212 support an external 16 MHz clock input and generate a 12.288 MHz clock for BCLK via its internal…
Part Number: TAC5212
We are using Analog MEMs mic (two ) in differenctial mode. please suggest the headphoen output
Shall we increase the C36/C38 to 470uf?
will these cap 470 µF will be electrolytic/tantalum/ Low-ESR aluminium/polymer, ≥ 6.3 V…
Part Number: TAC5212 We plan to use the TAC5212 in our custom communication system (5-100 kHz, low signal level, noisy environment).
I have done an initial quick test with the TAC5212-EVM, but clearly this is a device with many options and adjustments…
Part Number: TAC5212 Followed the documentation and got an error
set switch :amixer -c 0 cset iface=MIXER,name='ASI_TX_CH1_EN Switch' on
The Powerpoint file (in the git docs) show
– #amixer -c [card id] cset numid=[id],iface=MIXER,name='ASI_TX_CH1_EN…
Part Number: TAC5212 Other Parts Discussed in Thread: TAS5815 , Tool/software: Hi,
Kindly support to share Verb table for both Audio Codec (TAC5212IRGER) and Amplifier (TAS5815PWPR) as it is required for our software team.
Also, please share us the…
Part Number: TAC5212 Other Parts Discussed in Thread: AM5728 , PCM3168 , , PCM3168A
Tool/software:
Hi,
Could you please provide the reference design to interface with the AM5728 with the TAC5212 or PCM3168 Codec.
Please let me know if any challenges…
Part Number: TAC5212-Q1 Other Parts Discussed in Thread: TAC5212 , PCM5122 , PCM5242 , TAA5212 , TAD5212 Tool/software: Dears,
we would use the TAC5212 for our systems. We have a digital input (I2S) and we would use dac to have an analog differential…