Part Number: TAS2505 I am using TAS2505 for my speaker driver.
I want to connect 2 codecs, thus have to use 4 time slots.
I basically generated the I2S signal exactly as Figure 3-15 of SLAU472C (TAS2505 Application Reference Guide). WCLK = 16K. BCLK…
Part Number: TAS2505 Hello
TAS2505 Internal pull-up resistance
What is the internal resistance value between the RST terminal and IOVDD on the TAS2505 ?
Part Number: TAS2505 I have two TAS2505 chips, the one on the left works well while the one on the right does not. In 1.6k samples we have had around 5% failure rate with the audio chip. [Left - TI 291 A497B ----------------------- Right - TI 221 A7LTB…
Part Number: TAS2505 In the datasheet table for pin descriptions, Pin No.11 (SPKVSS) is listed with TYPE = "PWR" and annotated as "Class-D speaker driver power supply ground supply". However, in Figure 9-1 (Sample circuit) SPKVSS is shown connected to…
Part Number: TAS2505-Q1 Other Parts Discussed in Thread: TAS2505 Tool/software: Hello,
For TAS2505-Q1, according to the information in the EvalKit PDF, when a short-to-GND condition occurs, it is not recommended to repeat the reset process more than…
Part Number: TAS2505EVM Other Parts Discussed in Thread: TAS2505 , , TAS2020 Hello Texas Instruments Support Team,
I am currently working with the TAS2505 amplifier and have noticed a clear popping/clicking noise when powering down the amplifier after…
Part Number: TAS2505 Tool/software: Hi team,
Customer is using TAS2505. If the sampling rate is 22.05 kHz and the bit depth is 16 bits, how should the audio MCLK and BCLK be set? Can you provide the corresponding PLL register settings?
Thanks
X…
Part Number: TAS2505-Q1 Hi team,
When using the TAS2505-Q1, we observed during load short-circuit testing that a shorted load sometimes does not trigger the short-circuit protection.
The customer would like to know: What is the short-circuit impedance…