Part Number: TAS2505-Q1 Other Parts Discussed in Thread: TAS2505 Hi Expert,
Thanks a lot for your warm help!
My customer using TAS2505-Q1 in Auto Cockpit.
To meet ISO26262 standard, the FIT of TAS2505 must to meet 70%.
Is there any actions (like external…
Part Number: TAS2505-Q1 Other Parts Discussed in Thread: TAS2505 Hi team,
I'd like to know how to calculate the pull-up resistor for TAS2505 I2C SDA and SCL.
My customer wants to pull I2C up to IOVDD=3.3V with 4.7KΩ. The schematic in datasheet is 2…
Part Number: TAS2505-Q1 Other Parts Discussed in Thread: TAS2505 , Currently using the TAS2505-Q1 but we are not able to procure any at this time. It looks like the Automotive Diagnostics is the main difference between the TAS2505-Q1 and TAS2505. If we don…
Part Number: TAS2505-Q1 Other Parts Discussed in Thread: TAS2505 Hi TI team,
when power up, played READY souding, sometimes with "zizi" noise, using BCLK as PLL, DVDD and AVDD shared external 1.8V.
We have checked:
1. power supply sequence…
Part Number: TAS2505-Q1 Other Parts Discussed in Thread: TAS2505 Hi.
soc----I2S--->Tas2505---->spk.
I downloaded the tas2505 driver from TI's official website.
I can measure I2S data, such as PA_ I2S_ FS is 48Khz, PA_ I2S_ BCLK is 3.072Mhz…
Part Number: TAS2505-Q1 Other Parts Discussed in Thread: TAS2505
Hi, Support Team
Our customer Audio function use WM8960 will change to TAS2505-Q1
WM8960.pdf
Could help to Confirm I2S data DACLRC(WM8960) is WCLK(TAS2505-Q1) are the same?
WM8960
…
Part Number: TAS2505EVM Other Parts Discussed in Thread: TAS2505-Q1 , TAS2505
Tool/software:
==≈======================
My specifications and register settings
OutDAC: Class D
Input : TDM or I2S
Speaker load: 8Ω/2W
SPKVDD: 5V MCLK frequency: …
Part Number: TAS2505-Q1 Other Parts Discussed in Thread: TAS2505 ALL HI!
At present, tas2505-q1 is used for circuit design, 5V power supply drives 4 Ω / 2W horn. Is there schematic design and PCB layout reference? Please provide the design manual. thank…
Part Number: TAS2505-Q1 Hi team,
My customer have a question about how to handle with the LDO_SEL pin of TAS2505-Q1. Because in different versions of datasheet, one recommendation(FEBRUARY 2022) is connect to GND, one(OCTOBER 2018) is ties to either SPKVDD…
Part Number: TAS2505-Q1 Other Parts Discussed in Thread: TAS2505 Hello,
We encounter an odd issue for TAS2505 of I2C NACK.
When MCU sends Read / Write request to TAS2505(I2C addr 0x30), master
side just gets NACK or no response.
We checked power supply…