Part Number: TAS2560 Hi Sirs, My customer reported an issue of I2C rise time (2.979ns) and fall time (3.867ns) out of specification. The I2C clock rate is 315.8kHz. I think the faster rise time and fall time should be fine for the I2C communication, while…
3034.audio configuration.doc Hi Ivan
Now I used the same I2S stream with EVM board on our board to drive the TAS2560 on our board. It also have some noise. Any suggestions?
Part Number: TAS2560 Hi ti team,
When I was looking at the ti TAS2560 Datasheet, I did not understand PLL_CLK. The specification says The PLL output needs to be configured between 100 MHz and 200 MHz, but For example, PLL_CLK should be 49.152 MHz for…
Part Number: TAS2560 Hi tI team,
TAS2560 currently encounters the following problems:
1,At present, the data sheet we have got in hand, the register part is incomplete
As shown in the figure above, the related registers of book=0, page=50, 51, 52, book…
Part Number: TAS2560 Dear Team,
Customer configuring register in the TAS2560.
In the address 0x0F ,The sound is clean when value is 0x41 ,but there is a little of sound noise when value is 0x01 .
Customer hope BITCLK can provide a clean sound as MCLK,and…
Part Number: TAS2560 Dear Team,
We have DIN TAS2560 in customer side.
Could you help to reviewed schematic as below?
If you have any advise, please let me know.
Many Thanks
Jimmy
Hi Smith,
Do you have any further questions on this topic? Please let us know if your questions are solved so we can close this thread.
Thanks!
Best regards, -Ivan Salazar Applications Engineer - Low Power Audio & Actuators
Part Number: TAS2560
Hi Sirs, Would you please provide an example CFG to program the TAS2560 to send an IRQ# (either active high or low is fine) and assert error flags on CLK error of I2S ASI-1? Should we program the registers of 0x21, 0x22, 0x23, 0x4f…