Part Number: TAS2562 Other Parts Discussed in Thread: TAS2563 , TAS2557 , TAS2780 Hi,
Is it possible to use the TAS2562 I2S port as a master, where BCLK and FSYNC are outputs? If so, how is that configured? If not, why does the Pin Functions table on pages…
Part Number: TAS2562 What information does the TAS2562 provide via SDOUT? What are the consequences of not using this pin in a regular application?
Thank you!
Part Number: TAS2562 Other Parts Discussed in Thread: TAS2764 , TAS2780 , TAS2781 , TAS2557 , TAS2563 , Hi Team!
From my understanding, TI smart amps are able to pump more power through a speaker than the speaker is rated for. Say I have a 1W speaker, I believe…
Part Number: CC8530 Other Parts Discussed in Thread: TAS2562 , I am writing the xml configuration file to use the tas2562 with the cc8530. Is there a way to us an interrupt with the cc8530 in autonomous mode. My main concern is a UVLO fault of the TAS2562…
Part Number: TAS2562 hi expert,
In the application of the TAS2562, when playing at high volume, the output shutdown and then resumes after 1.4s. We grab the PVDD waveform as the picture show, at the pause moment, the PVDD achieved about 20V. It is used by…
Part Number: TAS2562 Dear TI support,
I try to use the internal tone generator of the TAS2562. Based on the datasheet, I made an analysis on the device configuration to generate a 1 kHz tone. However, I do not manage to get a signal at the output of the…
Part Number: TAS2562 Hi Sirs, Would you please advise the purpose of "tas2562-misc.c" in the TAS2562 Android driver package?
Thank you and Best regards, Wayne Chen 09/16/2020
Part Number: TAS2562 Other Parts Discussed in Thread: TAS2563 , , TAS2764
Hi team,
My customer is considering TAS2562/TAS2563, could you help me to answer the question below?
Does it have an automatic sleep / wake-up function like a "Noise Gate" at TAS2764…
Part Number: TAS2562 Hello Expert. I'd like to know about the specification of SDZ pin. Would you tell me following specifications? ・Sink current when SDZ is high? ・High level logic level's minimum value and typical value I'm looking forward to haring…
Part Number: TAS2562 Hi team, Good day.
Our customer is using the TAS2562 addon for PurePath Console 3 and found discrepancies between the software settings and datasheet as follows:
1. TAS2562 EVM Home -> Device Control -> Data Read -> Temperature: invalid…