Part Number: TPA6130A2 Other Parts Discussed in Thread: TAS2110 , TPA2011D1 , TAS2572 Tool/software: Hi ti team,
Please recommend an earphone amplifier IC with the following requirements:
Headphone amplifier requirements: 32 ohm load @ 450mW, Class D or…
Hi Richard,
You should look into our boosted amplifiers such as TAS2572. It supports 3V supply and up to 5.5V and features a boost to allow higher output power so 4W to 5W should be doable, take into consideration that the higher power required the higher…
Hi Masaru,
What is the load impedance? Please notice that at lower impedance the current demand increases, thus causing the voltage to drop. The boost in TAS2563 is 11V. The recently released TAS2572 offers a higher boost of 13V.
Best regards, -Ivan Sa…
Hello, Arthur,
Thank you for the quick answer.
TAS2572 seems to use IO supply voltage of 1.8V and 1.2V. Does TI have a device which can (a) i/o communication in 3.3V capable and (b) just activate with only power-on?
Best Regards, Masaru
Part Number: PUREPATHCONSOLE
Tool/software:
A table with links to all the software needed for audio devices and their EVMs. Find the device(s) of interest in the table and use the links to request access to the software you need.
Product or Part …