Part Number: TAS2770EVM Other Parts Discussed in Thread: TAS2770 , PUREPATHCONSOLE
Hi
We had purchased TAS2770 EVM for validating audio amplifier long days before. We requested PUREPATHCONSOLE 3 in the customer center of TI when we got EVM. But we are…
Part Number: TAS2770EVM I'm working with the TAS2770EVM and trying to use it in PDM mode. I'm generating the PDM data and clock in an FPGA and sending it to the amp via the PDM header on the eval board. Additionally, I've set what appear to be the appropriate…
Part Number: TAS2770EVM Other Parts Discussed in Thread: TAS2770 I am initially trying to send a signal to the amplifier and read out the voltage and signals using Audacity. I have tried several different combinations of USB audio settings as well as…
Part Number: TAS2770EVM Hello,
What is it that limits the TAS2770EVM input sample rates to 44.1 kHz / 48 kHz? I would like to test the amplifier in 192 kHz mode. Is there any way to do this with the EVM?
Thanks
Jim
Part Number: TAS2770EVM Other Parts Discussed in Thread: TAS2770 , Hi,
Now a customer is interested in SmartAmp device TAS2770. I have some questions about TAS2770EVM and PPC3 TAS2770 plug-in.
Q1. Does PPC3 TAS2770 app include Characterization tab? Q2. If…
Part Number: PP-SALB2-EVM Other Parts Discussed in Thread: TAS2770EVM , , TAS2557 , TAS2557EVM , TAS2770 , TAS2552 , TAS2562 , TAS2559 We have a TAS2770EVM which we use as an USB soundcard to read V/I-sensing signals into a PC. We need to get laser input signal…
Part Number: TAS5805MEVM Other Parts Discussed in Thread: TAS2770EVM , TAS5805M Hello,
I would like to request TAS5805MEVM Altium project (just like for TAS2770EVM), if is it possible to provide .
Best regards, Artur
Hello Jin,
Thanks for your reply.
After several unsuccessful tests on my card, now i plug in the eval TAS2770EVM card.
Now I can send the I2S signal generated by the NRF52832 of my card on the EVM I2S input connector and test different configuration using…
Yes, Even though TAS2770EVM is a Class-D amplifier, it can also be used to drive DC outputs by following the steps listed below:
Disable the HPF (located in Book 0, Page 0, Reg. address 0x04) by writing 0x00 to register 0x04
Attach a low-pass filter at…