Hi Guy
Henryk Zajdel said: root@deviant:~# cat /proc/asound/cards 0 [PCH ]: HDA-Intel - HDA Intel PCH HDA Intel PCH at 0x6001110000 irq 133
The log told me that you platform is the HDA archtecture. snd_soc_TAS2770 is the soc-codec driver, and it can…
Part Number: TAS2770EVM-STEREO Other Parts Discussed in Thread: TAS2770 , TAS2770EVM Tool/software: Dear colleagues;
I have a TAS2770 stereo amplifier running and checked using PPC3 and TAS2770EVM Stereo.
This is supposed to be controlled from the…
Part Number: TAS2770EVM-STEREO Other Parts Discussed in Thread: TAS2770 I am trying to connect purepathconsole3 with TAS2770EVM-STEREO board, but I get following message do I need different app in purepathcosole3 to support TAS2770EVM-STEREO board? If…
Part Number: TAS2770EVM-STEREO Other Parts Discussed in Thread: TAS2770 Hello Guys,
Good day.
Our customer is planning to buy the TAS2770EVM-STEREO. However, upon checking the user guide, he saw the note below and wanted to confirm if the fully released…
Part Number: TAS2770EVM-STEREO Other Parts Discussed in Thread: TAS2770 I was wondering if someone could provide some insight on the correct settings in order to receive current sense and voltage sense data in Audacity, using the setup of the Pure Path…
Part Number: TAS2770EVM-STEREO Other Parts Discussed in Thread: TAS2770 Hi,
I am interested in using the TAS2770 EVM to test a voice coil actuator, in which I will need to send DC voltages/non-audio waveforms to my actuator from the TAS2770 output.…
Part Number: TAS2770 I am working with a product that supports both 48kHz and 96kHz frame rates. Due to constraints in my SoC clock tree, I can only configure to provide a SBCLK/FS ratio of 64. I am using 16 bit samples with 32sclk slot sizes. When running…
Dear Luis:
Thanks for your letter!
The information about SoundWire is mentioned in the user's guide and datasheet that it's name is Tas2770(15w_smartamp_ivsense) ,as the following two attachments.
Thanks.
Best Regards
Dandan
tas2770(15w_smartamp_ivsense…
Hi Ivan,
Thanks for your response.
Yes, I can see in the PurePath Console that the Isense and Vsense are using two slots each. How is this working exactly for a mono amp? For example, if Isense is set to slots 0, 1, is the current always sent on…