Other Parts Discussed in Thread: TAS3108 Hello,
datasheet page 8 chap 3.7.1 describes missing EEPROM and access error as mentioned "No EEPROM is Present or Program Error Occurs".
How is this state detected? By CRC in the 10k firmware or the…
Other Parts Discussed in Thread: TAS3108 I have a TAS3108 EVM2. For some reason it looks like USB has to be attached before powering up the EVM or the program stored in EEPROM won't be loaded.
I tried the following:
A program is downloaded to the…
Other Parts Discussed in Thread: TAS3108 Hello,
I am using the Purepath Studio to confugure the TAS3108 part.
Kindly help to advise, if exporting the values of the runtime parameters from the PurePath™ Studio Graphical Development Environment, into a…
Other Parts Discussed in Thread: TAS3108 What are the advantages of using PEEK/POKE address and data commands verses a direct write or read to the I2C address? Also what is the correct format of the read command? I have learned a lot already from the I2C…
Other Parts Discussed in Thread: TAS3108 1) We were thinking of doing all the program (config) and coefficient (control) I2C interaction on the slave port. We believe the documentation supports this method but we just want to double check that we can do…
Thomas, Neil,
I've moved the post to the following thread as this issue is unrelated to the current Subject Line of 'TAS3108 fast enough?" Please move discussions / questions to the below thread to reduce confusion.
http://e2e.ti.com…
Other Parts Discussed in Thread: TAS3108 , PUREPATHSTUDIO Hallo everybody.
I am searching for PurePath Studio which support TAS3108 device (Frameworks).
From my first request I received from TI guy version "setup_PurePath_Studio_Portable_Audio_v4.10_build1_rev8749…
Other Parts Discussed in Thread: TAS3108 Hi, I'm trying to find D-Class Amplifier including DSP like TAS5825.
However, I would like to use TAS series without Host controller.
10 years ago, there was TAS3108, it was possible to boot with EEPROM.
Does…
Other Parts Discussed in Thread: TAS3108 Hy,
I use the TAS3108EVM2 and Input-Usb (A759) board, and I want to use the digital input with different sample rates. My questions is:
How the dynamic sample rate change works in TAS3108? How I can change…
Other Parts Discussed in Thread: TAS3204 , TAS3108 Hello everyone!
When I program the TAS3204´s SAP in the I²C Registers like the TAS3108´s SAP can I than get 32bit data or even TDM? - I would need some more in and out channels.
Thanks…