Hi there,
when I alter the frequency of the flexi tonegenerator during running in PPS on TAS3204-EVM two or three times no tone is produced any more.
Any idea?
Also I will have to alter the tone generator frequency by MCU via I2C. How does a frequency…
Other Parts Discussed in Thread: TAS3204 Hello: I am passing along these inquiries from my customer:
>>>> For single ended (RCA) inputs, I want to make sure that there are no issues with using the TAS3204 ADC in single ended mode. The EVM uses an extra…
Other Parts Discussed in Thread: PCM3070 , TAS3204 , TLV320AIC3254 Hey there,
I can't really see much useful information on the miniDSP cores used in the PCM3070 and how they relate functionally compared to the TAS3024 that it is supposed to be replacing…
Other Parts Discussed in Thread: TAS3204 , TAS5611 Dear Suzan,
I have a noise problem using the TAS3204:
In order to get a hight output from the TAS5611 I have to amplify the signal coming from the TAS3204EVM by 4 giving me a unacceptable high noise…
Other Parts Discussed in Thread: TAS3204 Dear ladies and gentleman,
I have a short question regarding the valid signals ranges for the analog inputs of a tas3204 DSP. Since the DSP is running from a single supply voltage I would have expected that…
Other Parts Discussed in Thread: TAS3204 Dear ladies and gentleman,
I'm trying for quiet a time now to get a TAS3204 DSP working and after some discarded pcb layouts I finally produced a layout with low noise and a working TAS3204. Or at least I believe…
Other Parts Discussed in Thread: TAS3204 , TLV320AIC3254 , TAS5548 Hi,
I need the schematic of TAS3204 Eval board. Can someone please post it?
thanks
Michael
Other Parts Discussed in Thread: TAS3204 Hi,
I am trying to get the following scheme working in TAS3204:
TAS3204 has been configured to run in slave mode. I have generated the code (attached) using PurePath Studio GDE (version 1.88 build 5) and…
Other Parts Discussed in Thread: TAS3204 When using the standard ToneGen from PurePath together with a TAS3204 device we found out, that the amplitude is going down over a period of time. It does not occur immediately. But when waiting e.g. 24 hours it…
Other Parts Discussed in Thread: TAS3204 Hey there,
We have a design that uses two TAS3204 chips, and it's having trouble passing C.E. in the emitted RFI test, specifically with an RCA attached, at 135mhz we're between 5 and 10 dB over the acceptable…