Other Parts Discussed in Thread: TAS5631 , TAS5162 In an multichannel application where we usually use TAS5631, I tried the TAS5162 in 1N PBTL mode.
Because I wanted to use only 2 inductors (18A -15uH gapped ferrite) I hardwired outA to outB and outC to…
I was wondering why the distortion measurements in the datasheets of the digital power amplifiers are allways specified with 2.5dB gain in the modulator. Does the modulator have a significant contribution to the measured distortion near full scale in…
Other Parts Discussed in Thread: TAS5162 , TAS5624A Hi all.
There is a question about processing of the "empty pin(not used pin)" in not using channel of TAS5162.
TAS5162 device is the amplifier containing four channel. What do we do with empty…
Other Parts Discussed in Thread: TAS5631 , TAS5614A , TAS5518 , TAS5162 On the mode control in the data sheet it lists AD/BD modulation. It is either AD or BD isn't it. Which is it? I don't see another select to pick which one.
MODE PINS PWM INPUT…
Other Parts Discussed in Thread: TAS5162 , TAS5352 , TAS5631 Dear, Sir.
I have an simple question regarding TAS5162.
"BTL/PBTL-Configration Pulldown Resistor" is located on each outputs(OUTA/B/C/D).
These are described the block diagram on…
Other Parts Discussed in Thread: PCM1808 , TAS5086 , TAS5162 , DIR9001 , TAS5162DKD6EVM , PLL1705 Hello!
a year ago I designed a class-D amplifier based on the TAS5162, pcm1808 and TAS5086. During the year, was made a few hundred samples intended to be sold…
Part Number: LM5116 Other Parts Discussed in Thread: TPS51125 , TAS5162 , TAS5518 Hello. I have an issue with LM5116 giving me as thread says low and unstable output voltage. I made my pcb following the schematic from http://www.ti.com/lit/ug/snva285a/snva285a…
Other Parts Discussed in Thread: TAS5631B , TAS5162 , TAS5631 Hi all,
Since 2 years we manufacture an eight channel amplifier unit using 4 pcs TAS5631B on one board. In general, specifications are ok and reliability is no issue either. However a strange…
Hi Don,
thnx for the quick reply.
We use 48V as power bus voltage....which is too high for TAS5614 and 5624. ( if the datasheet is correct)
The options that are left are the TAS5631 and the TAS5162 which are capable of operating on 48V.
I wanted to use…
Other Parts Discussed in Thread: TAS5518 , TAS5631 , TAS5508C , TAS5518C , TAS5631B I am using a TAS5518 to provide PWM to the TAS5162 . I don't see a setting on the TAS5518 to pick AD or BD. I have a design update using a TAS5631 were you can chose AD or BD…