Peter,
Please see the CAD files (scroll down on the following link) for a device that shares the same package as the DRV8432:
http://www.ti.com/product/tas5162
Other Parts Discussed in Thread: TAS5713 , TAS5711 , TAS5162 Hi!
I'm planning of using a TAS5713 in a project of mine and have a question about the startup sequence:
Why do you need to raise the PVDD after DVDD and what happens if you don't?
…
Other Parts Discussed in Thread: TAS5631 , TAS3308 , TAS5342 , TAS5162 Hi
I plan to use the TAS5631 drived by a TAS3308 DSP in a single ended configuration, the TAS3308 have a special startup sequence for SE configuration called mid-z, i want to know if…
Other Parts Discussed in Thread: TAS5342L , TAS5352 , TAS5162 The TI specs on the TAS5342L states that the absolute max PVDD is 46v yet in the recommended operating conditions you indicate PVDD typ is 32v and max is 34v. What happens between 34v and 46v…
Other Parts Discussed in Thread: TAS5615 , TAS5162 Hi the
I nticed that precious post ( http://e2e.ti.com/support/amplifiers/audio_amplifiers/f/6/t/28843.aspx ) specifies how to setp the the TAS5162 in the event only one half of the outputs are being used…
Other Parts Discussed in Thread: TAS5631 , TAS5630 , TAS5162 Hi,
Currently we are evaluating a new design incorporating the TAS5631.
We use the DKD version, 2 x BTL at 48V. AD modulation scheme
At 3.5 Ohms load, some 2dB before clipping, spikes apear…
Hi Don,
many thanks sofar,
using this we can get at least below the 300K, in combination with proper gate drivers
it seems feasible. Some other question instead...
we switched from TAS5162 to TAS5631 in a new design. This because we needed t…