Part Number: TAS5342LA Hi,
A customer's product will supply 32V to PVDD even if VDD power is not supplied. In this state they call standby mode, the MPU power is supplied, but almost circuits including PWM output stop operating. Is there any problem…
Part Number: TAS5342LA Other Parts Discussed in Thread: OPA320 Hi,
If using TAS5342LA as a mono BTL, can we eliminate all passive parts of unused channels?
Best regards,
Akio Ito
Part Number: TAS5342LA I want to improve the thermal conductivity on existing design by using metal-based thermal grease instead of an insulating TIM.
The datasheet does not show if an electrical connection to any net is allowed for the thermal pad…
Part Number: TAS5342LA Hi
When BD port is not used, how to care about capacitor between PVDD and GVDD? Should it be implemented?
( I pointed out with red frame)
I appreciate if you could reply.
BestRegards
Part Number: TAS5342LA Hi,
A customer wants to get a 100W output at 5 ohm load by TAS5342LA in BTL or PBTL setting. He requires 'Output power vs supply voltage' data in BTL and PBTL, and the efficiency data in PBTL. Would you measure the datum if TI…
Part Number: TAS5342LA Hi
I have a question related to the following post.
I would like to use TAS5342LA with disabling C and D port.
Holding ~RESET_CD low will keep the OUT_CD in Hi-Z. 1. In that state, is it no problem OUT_C and OUT_D are…
Part Number: TAS5342LA Hi
Is it likely that difference of PVDD would affect to Tc (case temperature) of the device in spite of same output power?
For example,
1. PVDD =12V, L/R has 12W/12W, that leads Tc=80C (Ta = 25C) 2. PVDD=19V, L/R has 12W…
Part Number: TAS5342LA
Hi
Regarding to the datasheet,IVDD(typ) is 7.1mA, IVDD(max) is 17mA at operating 50% duty cycle.
1.
What is the meaning of condition of operating 50% duty cycle? Is the condition of the pwm input?
2.
IVDD(max)…
Part Number: TAS5342LA Hi
Is there any problem for applying PWM input to TAS5342LA before de-asserting RESET?
Or is this sequence not matter?
BestRegards