Part Number: TAS5342LA Hi
I have a question related to the following post.
I would like to use TAS5342LA with disabling C and D port.
Holding ~RESET_CD low will keep the OUT_CD in Hi-Z. 1. In that state, is it no problem OUT_C and OUT_D are left open…
Other Parts Discussed in Thread: TAS5342LA Hi
We have question about the overcurrent limit protection of TAS5342LA.
We can refer the following description on the datasheet.
IOC=8.4A(typ) Resistor-programmable, high-end, ROC=22Kohm with 1ms pulse, Tc=75…
Hi
Do you have information of allowable power dissipation on the datasheet test condition?
Actually, the power dissipation would be affected by output circuit (like inducors).
However, we want to confirm the variability of the power dissipation (especially…
Other Parts Discussed in Thread: TAS5342LA , TPA3250 , TPA3251 , TPA3244 , TPA3245 , TAS5132 Hi
TAS5342LA offers mode selection of BTL mode and PBTL mode, but we couldn't determine if it supports both AD modulation and BD modulation.
Can we use TAS5342LA…
Other Parts Discussed in Thread: TAS5342LA Hi
We have question of TAS5342LA.
We are going to use this device with BD, but according to datasheet, TAS5342LA had been tested with AD modulation. Also, the reference schematic is described in AD.
1. Where can…
Other Parts Discussed in Thread: TAS5342LA , TAS5132 , TAS5342 Hi
We are about to evaluate TAS5342LA and TAS5132 using EVM.
So, we have following questions.
1. We found TAS5342LDDV6 EVM but it seems TAS5342LA is not mounted on the board.
To evaluate TAS5342LA…
Hi
We want to know the MAX current according to OC-adjust register value 27kOhm.
Because we can refer 27kOhm as OC-adjust register value from typical application schematics on the datasheet.
Figure 14/Figure 15/Figure 17/Figure 18
www.ti.com/.../tas5342la…
Other Parts Discussed in Thread: TAS5342LA Hi
We want to know the state of the following pins of the TAS5342LA when PWM activity detector is active.
Do you have a solution?
1. SD/OTW pin
2. Output pins
3. When PWM signal is lost and then recovered, how…
Other Parts Discussed in Thread: TAS5612LA , TAS5342LA Customer study using same DSP (BD mode) input to TAS5612LA, then switch to TAS5342LA with the same DSP PWM output, the level is lower by 7dB.
Both TAS5612LA and TAS5342LA are used in BTL mode.
DSP (BD…