Part Number: TAS5411-Q1
1 Is it possible to write 0xBF to the address 0x03? When writing the value of 0xBF to the actual prototype, some prototypes make sounds while some don't.
2 In addition, how is the setting of the 0x03 register defined? Are…
Part Number: TAS5411-Q1 Hi team:
We use a 1A regulator for the power supply of TAS5411, but we found the external speaker could cause 2A@5ms inrush current while starting to play a audio file, which cause regulator's over current protection.
We are…
Part Number: TAS5411-Q1 Other Parts Discussed in Thread: TLV320AIC3104-Q1 , TAS5431-Q1 , TPD3S714-Q1 Dear Team,
Could you help to check does TAS5411-Q1 can meet spec as below?
Speaker interface: The emergency call module requires a built-in audio amplifier…
Part Number: TAS5411-Q1
Hi, Support Team
we use TAS5411-Q1 and default is 26db and input capacitance is 1uF.
if setting gain from 26db to 36db, and keep input capactance is 1uf, have any side effect?
Could possible trigger overcurrent protection?
if…
Part Number: TAS5411-Q1 Other Parts Discussed in Thread: TAS5411Q1EVM
Hi, Support Team
we test PVDD is13v and drop voltage to 4.2v, that can trigger "PVDD undervoltage fault register, but if PVDD is 5v drop to 4v that cannot trigger "PVDD undervoltage…
Part Number: TAS5411-Q1 Hello team,
My customer is using TAS5411EVM board to drive the 4Ohm speaker, but the tool report the short-to-GND fault. The detail is as below:
Supply of EVM board, 12.6V
Speaker is 4 Ω,they measured as 4.1 Ω.
Please…
Part Number: TAS5411-Q1 Other Parts Discussed in Thread: TAS5431-Q1 Dear Team,
I am new to use audio amplifier design to drive speaker. We are using 3W, 4 Ohm speaker for Audio ecall in automotive environment. Need to know if it is ok to drive 3W speaker…
Part Number: TAS5411-Q1 Hi, team,
I posted one question about TAS5411-Q1 SpeakerGuard, below is reply.
https://e2e.ti.com/support/audio-group/audio/f/audio-forum/1065274/tas5411-q1-speakerguard-questions?tisearch=e2e-sitesearch&keymatch=tas5411#
…
Part Number: TAS5411-Q1 We are using TI TAS5411-Q1 on our Cluster Product for Playing different tones.
The Input to the amplifier is connected to DAC output through Bandpass filter (LPF and HPF in Series) the interface at the input of Amplifier is single…
Part Number: TAS5411-Q1 Hi team,
Could you check if NVM such as OTP memory is integrated for TAS5411QPWPRQ1? We received this question from the customer.
Kind regards,
Shota