Part Number: TAS5414C Hello,
My customer is asking about PBTL on TAS5414C.
Their requirement items are following.
Power supply: 13V
Output(Mono) : 60W (THD+N 1%), 4ohm
They are considering adding an extra connection as a PBTL to unused output…
Part Number: TAS5414C Hello, My customer is asking about mute pin(2pin) in TAS5414C.
They want to unmute the audio as soon as possible to prevent the beginning of the sound being cut off. (Within 10ms after sending the I2C command)
If the pop noise…
Part Number: TAS5414C Hi
The customer can capture the I2C Address, but after passing the front-end codec output to the tas5414c input, the tas5414c also does not output sound, but it is confirmed that the codec output has sound output.
Do I need to…
Part Number: TAS5414C Other Parts Discussed in Thread: , TAS5414A , TPA6404-Q1 Hello,
My customer is asking about TAS5414C at PBLTL mode(mono).
1) Can TAS5414C output with following connection?
Conditions:
DC supply(PVDD): 12V、
Speaker: load…
Part Number: TAS5414C-Q1 Other Parts Discussed in Thread: TAS6754-Q1 Tool/software: Hello,TI teams,
I am gonna evaluating TAS6754-Q1 EVM.But it is not formal materials,so I have to use TAS5414C-Q1 for insteading.
I have already install the PPC3 to…
Part Number: TAS5414C Hi
One question is about TAS5414CPHD What is the usage specification of Dual Inductor in the circuit diagram? I see that there is no description in the public version circuit and BOM
Part Number: TAS5414C-Q1 Dear. Experts.
I am using the TAS5414CQ1(silked on chip as XTAS5414CQ1) as the master. I have some problems.
1. In the Play All or Mute All state, pop noise occurs when controlling individual channels as shown below.(and vice…
Part Number: TAS5414C Hi sir,
I have a inquiry on the Parts difference between TAS5414C-Q1 and TAS5414C.
Generally, TI automotive grade devices have -Q1 suffix.
But the datasheet for TAS5414C is also mentions it as automotive device.
I would like…
Part Number: TAS5414C-Q1 # Issue: I can't R/W the SLAVE AMP (only used salve2). But MASTER R/W reg. are OK (except reg. 0x0A can't set to 0x40).
# My initial sequence:
Read from master register 0x00 => value = 0x00
Read from master register 0x01…
Part Number: TAS5414C-Q1 The amp chip in question is used in the Sony MEX-XB1000BT car radio. This car radio has a problem: it turns off and resets every time the volume is turned to maximum, even if the car radio is connected directly to the 12V battery…