Part Number: TAS5424A Hi,
Is there information somewhere making clear what the changes were between the TAS5424, TAS5424A, B, & C versions?
In these days of parts shortages it necessary to understand what has changed as this part has been updated…
Part Number: TAS5424A Hi all,
I really have a hard time getting this amplifier to work. Tried following this post e2e.ti.com/.../53445 but so far without result. Also, the thing I'm observing is that my initial check of 0x00 reports 1110000 which according…
Part Number: TAS5424A We produce a product using 2 of the TAS5424 power amplifiers. We have several thousand in service. On 2 or 3 occasions we have had a return where all 4 of the speakers attached to one of the power amps ICs were burnt in the voice…
Part Number: TAS5424B-Q1 Hi,
We have been using the TAS5424A for many years in a design without any issues. I recently decided to try installing the TAS5424B in its place because we may need to raise the supply voltage to 24V. The B version would not…
Part Number: TAS5424A Support Path: /Product/Development and troubleshooting/Find key information on a device/ Hello, which is the difference between this two part numbers? They differ only with the "M" letter, but i can't find in the datasheet or in the…
Part Number: TAS5424A Hi,
I have an application with a load impedance of 1 Ohms that need around 50 Watts. In datasheet TAS5412 is "even one 1 ohm load by paralleling BTL channels". How can I connect the outputs to PBTL? Can I use 4 channels…
Other Parts Discussed in Thread: TAS5424C-Q1 , TAS5414C-Q1 Dear sir,
now we are looking for an TAS5424A 4 channel amplifier, how do we interface with rasberi-pi model, in I2C commounication.
All,
My customer is currently using the TAS5424A (four channel Class D amplifier). They want to migrate to the TAS5424C. The two parts are pin for pin compatible. The TAS5424A uses a PVDD rail of 21V and the TAS5424C uses 24V. If they can run the part…
Other Parts Discussed in Thread: TAS5414A Hi,
We are using the TAS5424A amplifier in our hybrid stepper motor design. We have the amplifier DC coupled from a DAC and some op-amp filtering/differential amp.
We set up the I2C registers as follows:
* Clear…
What I am looking for is a "Fader" function and an amplifier.
Page 26 of the TAS5424A Amplifier spec shows fixed gains(12,20,32 db) for each speaker. I there a way to vary these so it can be used as a "fader" function?
Or, how do you…