Hi Adam,
Thanks for your response!
When we connect the both device(TAS5508 & PCM1808), which one will be working as master? As mentioned in the datasheet TAS5508C is a clocked slave-only device.
The TAS5508C receives MCLK, SCLK, and LRCLK from other…
Other Parts Discussed in Thread: TAS5614LA , TAS5508C , TAS5508 Hi Engineers,
I plan to connect TAS5508C and TAS5614LA (BTL).
In this case, which channel configuration register value on TAS5508 is recommend?
Regards,
Hello Luis,
Yes I can see that. Will you be able to recommend product that can independently adjust frequencies of outputs. I know TAS5508 is used for this type of work. Is this product capable of battery powered applications (portable devices)?
Thanks…
Hello Mike-san,
Thank you for your reply.
I was looking at this report, but had missed the statement below.
”After installing the PurePath Console GUI, add TAS5612 plug-in to the Target Selection and Open the TAS5612 GUI.”
I will tell this…
Maybe we have the different access. i can't find the TAS5558 GUI.
I used the TAS5508 GUI and ALE 5.2 for TAS5508. I want these two tools for TAS5558.
Thanks
Hi Don,
Thank you for your advice. Just to clarify, that means I can simply use TAS5508/TAS5518 GUI with this board to control those chips?. Do I have to load the firmware to the USB board or can I run directly TAS5508/TAS5518 GUI from the PC to communicate…
Other Parts Discussed in Thread: TAS5548 , TAS5508 Hello
Customer intends to use TAS5548.
Customer pointed out that there are PCB layout in the TAS5548 EVM slou351b.pdf.
According to that document, PLL ground #5 pin is connceted to DVSS with trace ( 0 ohm…
Hi Don Dapkus,
Would you suggest how to set DRC for TAS5508 GUI ?
I use ALE to generate a DRC file for TAS5508 GUI and load it, can't see any effect ?
Many thanks a lot !