Part Number: TAS5634EVM Other Parts Discussed in Thread: TAS5558 , Hello, I have the TAS5634EVM and want to evaluate especially the capabilities of TAS5558.
I could not find any description on the programs P0, P1 and P2 that I can select via the button PROGRAM…
Other Parts Discussed in Thread: TAS5558 , TAS5548 Dear Sirs,
My customer asked me about BEQ coefficient setting by fs change of TAS5558
Select the TAS5548 / 58 in PPC1.16 of target. Then, when you open the sample rate, it will be displayed only 96,176.4…
Part Number: TAS5624ADDVEVM Other Parts Discussed in Thread: TAS5558 , TAS5624A , , TAS5612A , TAS5624 I have a TAS5624ADDVEVM which I would like to use to evaluate TAS5558 and TAS5624A.
I am aware that the documentation recommends to use "TAS55XX GUI" as…
Other Parts Discussed in Thread: TAS5558 , TAS5631B Hello, My name is Bill and I'm an Engineering student using the TAS5558 PWM chip with a TAS5631B Power Stage.
We're using a USB miniStreamer from MiniDSP to send Audio into the TAS5558. We were…
Other Parts Discussed in Thread: TAS5548 , SRC4190 Hi,
Could you please tell us the group delay when using TAS5548/58 with the ASRC ? For instance, the group delay is mentioned in the data sheet of SRC4190 as below. The group delay is 2.52ms(102.53125/fsin…
Meanwhile I set up to use the I²S input in order to play other samplerates, which works. But this unfortunately limits the use of the EVM as I need another PCB to provide that data. A bit of a pitty. Especially as it seems to be no hardware, but MCU FW…
Other Parts Discussed in Thread: TAS5558 , TAS5538 Dear Sirs,
My customer asked us about allowable variation range of fs input of TAS5558.
If I2S input Fs from the previous stage circuit was 44.5kHz and 47.1kHz, It works by decoding properly?
Best Regards…
Other Parts Discussed in Thread: TAS5558 , TAS5538 , TAS5612A Dear Sirs,
My customer asked me as below question.
Please tell me whether there is a difference between the residual noise at the input LRCK Fs = 44.1KHz and 48KHz setting under the following…
Other Parts Discussed in Thread: TAS5558 , TAS3108 , TMS320C5505 HI, I am looking for a way to route / mix 4 I2S inputs down to 1 I2S output L/R ( 8 - 2 mixer ) and would like completely flexible mixing possibility's.
for instance I would like to mix…
Hello Justin-san,
My customer asked us additional question.
Please tell me how to output the SDIN2 only to SDOUT.
Then I think following setting.
1.TAS5558 setting
1) resister (0x04) D0⇒1
2) resister (0xC5) D24⇒0,D25⇒1
Please tell me how to…