Hi
I'm a electronic engineer student, I'm from Colombia, I have made my own PCB for the IC , but it worked only few times.
I used all the considerations in the datasheet and bought the components according the user guide of the evaluation module…
Other Parts Discussed in Thread: TAS5611A , TAS5630B I want to use the TAS5611A in the 2.1 configuration (mode bits M[3:1] == 011, 1 × BTL +2 ×SE). But I can't find in the datasheet which inputs A-D are used for the BTL channel, and which are used for the…
Other Parts Discussed in Thread: TAS5611A Hi,
We are using the TAS5611A in a configuration where there is a transformer at the end of the smoothing filter. The op smoothing filter is more or less the same as that of the EVM circuit of this device. We have…
Other Parts Discussed in Thread: TAS5611A Hello,
I have sketch a picture of the error reporting of the TAS5611A. Is it correct?
http://www.ti.com/lit/ds/symlink/tas5611a.pdf
Thank you for your help.
Other Parts Discussed in Thread: TAS5611A Hello,
Im using the the amplifier TAS5611A with AD modulation.
1. I dont understand, how the feedback loop works.On the internet I found a picture, with the principle, but I dont know if its right.
2. If I have…
Other Parts Discussed in Thread: TAS5611A Hello,
I have a question to the overcurrent limit protection on page 10 in the datasheet: http://www.ti.com/lit/ds/symlink/tas5611a.pdf .
1. What is the difference between I OC and I OC_LATCH ? I have found:
"In situations…
Other Parts Discussed in Thread: TAS5611A Hi,
I am trying to calculate the current consumption from the 12V rail by the TAS5611A. From the data sheet I seem to calculate a total of 100mA. Is this correct. I need to be sure as I have to do a secondary…
Other Parts Discussed in Thread: TAS5611A Hi,
It seems like the pin define 49-60 for TAS5611A's .bxl file which shown on TI.com is incorrect.
Could you please check it or send me the new one?
Thank you.
Mister Lei
1/22/2013
Other Parts Discussed in Thread: TAS5414B-Q1 , TAS5611A Hi,
Would you perform the following evaluations?
My customer wants a result by this week.
-----------------------
<condition>
・PVcc=24V
・RL=4Ω
・BTL
・Input Wave = Square wave
・Output Wave…
Other Parts Discussed in Thread: TAS5611A Hello There was a problem with power supply TAS5611A when it lights up dressing up SD. PVDD=30V/16A, VDD=12V InA,B,C,D=3.5V, OUT A=9V OUT B=650mV OUT C,D=9V MODE SELECTION PINS Differential 2 × BTL BD mode. In…