Other Parts Discussed in Thread: TAS5614A , TAS5624A , TAS5614LA Hi,
Could you please send us the data such as the graph which is mentioned on page 11 of TAS5614A data sheet since we could not find the graph of "Output Power vs Supply Voltage" for the single…
Other Parts Discussed in Thread: TAS5614A We wish to use TAS5614A in a non-audio time division multplexed application which requires floating the outputs when disabled and having active outputs within 200uS of enable (via /reset going high) We are using…
Other Parts Discussed in Thread: TAS5614 , TAS5614A , TAS5518C I like to use TAS5614A in project. But only TAS5614 is available small time now. Can I use TAS5614 instead of TAS5614A first time?
PWM contoller will be TAS5518C
Other Parts Discussed in Thread: TAS5518 , TAS5614 TAS5518 can regulate volume with modulation of power supply voltage of output stage. It is very good. But I read datasheet on TAS5614 recomendate voltage supply between 18 and 36 V. It is only 6 dB of volume…
Part Number: TAS5548 Other Parts Discussed in Thread: TAS5614A Dear all,
If I select the lowest possible value for the modulation index (xFF in register x16, hence a modulation index of 87.40% for channels 1 and 2), can I expect a limitation of the output…
Part Number: TAS5631B TAS5614A
Hi,
I designed a TAS5631DKDR Board for Single-Ended Application and a TAS5631BPHDR Board for BTL Application, both designs‘ schematic diagram are the same as the recommend design in the Users' guide. But I met the same questions…
Other Parts Discussed in Thread: TAS5612LA , TAS5614LA , TAS5624A , TAS5612A , TAS5614A , TAS5630B Hi,
TAS5612LA, TAS5614LA and TAS5624A datasheet have description "The TAS56xx uses constant voltage gain" in first page. Though TAS5612A and TAS5614A…
Other Parts Discussed in Thread: TAS5613 , TAS5614A Hello,
I'm searching for the package PHD S-PQFP-G64 for eagle. I can't find it in any library.
Please help me!
Other Parts Discussed in Thread: TAS5558 , PCM3070 , DIR9001 , TAS5631 , TAS5631B , TAS5614A , TAS5548 , TAS5614LA Hello,
I use a tas5558 with bd modulation (because the outputfilter of my class d amp is designed for bd modulation). Unfortunately there is a high…
Other Parts Discussed in Thread: TAS5518 , TAS5614A , TAS5631 , TAS5614 , TAS5508C , TAS5518C State:
TAS5518 & TAS5614A at 192 or 176.4 kHz. All biquads switched off. DRC switchted off. Louness switched off. Only amplification control is used.
I want…