Part Number: TAS5614LA Other Parts Discussed in Thread: TAS5614A Hello,
The question is in the title.
All I could notice reading the manuals is that the LA is slightly better in terms of THD.
Any other major advantages for the LA?
The 5614A is…
Part Number: TAS5614LA Other Parts Discussed in Thread: TAS5614A Sorry if this is a duplicate, but my previous message was not acknowledged by your system. So here we go again.
Does the TA5614LA offer signifcant advantages over the TAS5614A?
All I…
Part Number: TAS5614LA
Hi,
Could you please provide the recommended torque(min/typ/max) to tighten the M3 screws to the heatsink for HTSSOP package ? In addition, would you please tell me the side effects if the torque is extremely low or high ? …
Hello Ito-san.
The major difference is that 1N only supports AD modulation where 2N supports both AD and BD modulation.
Since the BTL output of a class-D requires 2 half bridges, 2 PWM signals are needed to drive the output FETs in the power stage…
Other Parts Discussed in Thread: TAS5614LA , TAS5624A Hi,
Our customers would like to know the difference of TAS5614LA and TAS5624A. We believe that this difference is only RDSon physically as below. Therefore, the idle power and the efficiency also…
Other Parts Discussed in Thread: TAS5614LA Hi team,
A question about operation temperature range of TAS5614LA. At the end of datasheet, 'PACKAGE INFORMATION' section, it said the OP TEMP is -40°C to +125°C. While in section 'Absolute Maximum Ratings…
Hello,
For the TAS5614LA it is recommended to use 4 inductors in PBTL. For high power devices this is generally the case to avoid current spikes and shoot through on output bridge due to small variances in the timing and properties of the paralleled…
Hello,
Yes this is correct.
For THD+N measurements, it is standard practice in audio to look at harmonic content without any filters in the audio band to assess amplifier linearity. Since A-weighting effects the audible band it is not used. Instead…
Other Parts Discussed in Thread: TAS5614LA Hi,
When TAS5614LA configures as mode [3:1] = 001 (1N+1/2xBTL/AD mode), how do I treat unused input pin such as INPUTB and INPUTD?
i.g. connect to GND via pull down resistor approx. 47kohm and so on...…