Part Number: TAS5630B Other Parts Discussed in Thread: TPA3255 Dear Sir.
Our company used TAS5630B DKD Chip before.
Anyway Now we need TAS5630B Chip for the product our ITEM.
But TAS5630B Chip's heatsink looks like used product.
Our supplier…
Part Number: TAS5630B Other Parts Discussed in Thread: TPA3221 Hi,
Good day,
I have been study TAS5630B and TPA3221 Audio Amp differences for my recent project.
I find out that TAS5630B has much higher price compared to TPA3221.
In term of Audio…
Part Number: TAS5630B Dears :
TAS5630B damaged in PP, total 100 PCS of 200, fail ratio is 50%. I found abnormal waveform on RESET PIN when switch Signal source , the voltage on RESET pin usually is 3.3V, but when did fast switch signal source ,the voltage…
Part Number: PCM1794A-Q1 Other Parts Discussed in Thread: TLV320DAC3100 , TAS5630 Hi Experts,
Good day. Sorry to bother you here but I would like to ask your assistance in selecting the right DAC for my client.
They are looking for a simple DAC device…
Part Number: TAS5630B Hi TI,
we are using TAS5630B in BTL mode; having 2 separate channels. The design is almost identical to the evaluation kit, but we have a 1:4 transformer connected to each output channel to get 100V. The nominal load at secondary…
Part Number: TAS5630B Hi TI,
we have a question regarding the overcurrent function (cycle by cycle) and the resistor Roc: Is it correct that this function changes depending on BTL and PBTL?
According to datasheet, if using 2 x BTL and max output is…
Part Number: TAS5630PHD2EVM Other Parts Discussed in Thread: TAS5630B Hi,
We have been using the TAS5630b in a product for 6 years and are now having issues with the device failing.
I am just wondering if any other customers are also experiencing…
Part Number: TAS5630B Dears,
We use TAS5630BPHDR to drive 2 speaker, during the using,some pcs occur damage.
we test the phenomenon is:
1. TAS5630B's four output PINS(OUT_A/B/C/D),one of them short to itself GND(GND_A/B/C/D).
2. PIN-17(/SD) assert…
Part Number: TAS5630B Hi, I have a design running at 30V that will not start up. Would it be possible to review the schematic and board layout to see if I have made an error in either?
I am trying to run in PBTL mode, I have tried to copy the evaluation…
Part Number: TAS5630B Hi TI, we are using TAS5630B as an audio amplifier on board ships. Because the maritime standards are setting a maximum limit for emitted noise, we have been forced to use expensive common mode coils. Because the standard sets a…