Part Number: TAS5634EVM Other Parts Discussed in Thread: TAS5558 , Hello, I have the TAS5634EVM and want to evaluate especially the capabilities of TAS5558.
I could not find any description on the programs P0, P1 and P2 that I can select via the button PROGRAM…
Part Number: TAS5634EVM Other Parts Discussed in Thread: TAS5558 , , PUREPATHCONSOLE , TAS5548 , DIX4192 , TAS5634 Hello, I have the TAS5634EVM and want to evaluate especially the capabilities of TAS5558. One important point is to test support of samplerates…
Part Number: TAS5634EVM Hello,
I’d like to test different ways to cool 4+ high power audio amps and would prefer to use the TAS5634EVM boards.
Is it possible to receive the Altium Designer files for TAS5634EVM?
Kind Regards
Part Number: TAS5634EVM
Hello,
One customer who used TAS5634EVM tested the SNR and THD+N, and he found that the results are different with the datasheet.
He used Pure path with default configuration, changed CH1 AD or BD modulation, used USB cable to…
Part Number: TAS5634EVM I am currently trying to program the TAS5634EVM through PPC V1.16. I have successfully flashed code onto it and it is operating within specifications. However, during my time of trying to implement my configuration with PPC v1.16…
Part Number: TAS5634EVM Other Parts Discussed in Thread: DIX4192 , TAS5634 , TAS5558
Is it possible to play more than 20Khz with EVM? (i.e. 30kHz~40kHz) In case of USB input, it is transmitted to the load by TAS1020B --> DIX4192 --> TAS5558-->TAS5634, and…
Part Number: TAS5634EVM I am now testing TAS5634EVM and found periodic noise on the OUTA~OUTD.
Test condition
- PVDD 50v
- Board Configuration : BTL
- Audio input : no
- ppc 1.1.6 : Do not run
- proving : oscilloscope ch1: OUTA , ch2 OUTB, math1: ch1…
Part Number: TAS5634EVM Other Parts Discussed in Thread: TAS5634 , DIX4192 Hi team, I have 4 units of TAS5634EVM. The 3 units works fine. The 1 units have problem. I have the User's Guide SLAU750–October 2017. The problem point is column of "2.3…
Part Number: TAS5634EVM Hi Team,
Could you please share me the Altium Designer files for TAS5634EVM ? My customer needs it to bulid the project. Thanks very much!
Part Number: TAS5634EVM Other Parts Discussed in Thread: TAS5634 , Hi sir,
My customer would like to test the class D amplifier TAS5634 performance, he would buy the TAS5634EVM BOARD , and he wanna which type of resistor for the EVM to load?
He would like…