Part Number: TAS5704 Hello, Is it possible to request for the ESD values of this device? It is mentioned in the datasheet that these devices have limited built-in ESD protection, but it seems there is no information on the exact values. Thank you!
Part Number: TAS5704 Hi Sirs, With 24V PVCC, 6.8ohm load, does 350uV noise floor make sense with the TAS5704? My customer's found 240uV noise floor ith most of their TAS5704 devices, however, there is one corner case with 350uV noise floor. We can duplicate…
Part Number: TAS5704 Which input channel is associated with which output channel? The device has SDIN1(Left,Right) and SDIN2(Left,Right), and outputs A, B, C, D. The datasheet doesn't map inputs to outputs.
Is SDIN1(Left) mapped to output A? SDIN1(Right…
Other Parts Discussed in Thread: TAS5760M , TAS5704 , TAS5766M Hi Sirs, We are comparing the Pout on the TAS5704, TAS5760M and TAS5766M EVM with the same test condition (24V, 6ohm load, I2S input = -2dBFS/6.7KHz). We found clipping with the TAS5760M with…
Other Parts Discussed in Thread: TAS5704 , TAS5760M , TAS5756M Hi Sirs, Would you pls assist us to generate official TAS5704 THD+N vs Pout curve all the way to 25W Pout with 6.8ohm load, 24.6V PVCC, -1.68dBFS I2S input? Than you and Best regards, Wayne…
Other Parts Discussed in Thread: TAS5704 When evaluating a prototype board, capacitor in LOOP Filter was damaged by short mode.(C1 47nF recomended in datasheet) I checked OUT_X waveform,it was duty50%.(I2S signal is input)
-Is this movement right behavior…
Other Parts Discussed in Thread: TAS5704 Hi,
Can we use TAS5704 like the attached connection?
(my customer'd like to know that TAS5704 can drive two 8Ω speaker in parallel per channel. )
If can, is there any point that they should care about?
…
Other Parts Discussed in Thread: TAS5704 Hi,
To compare the bulk capacitor value between TAS5704EVM and TAS5760EVM,
there is a big difference between them,
(TAS5704 needs 220uF for each 4 PVcc inputs / TAS5760 needs one 470uF.)
Why can TAS5760…
Other Parts Discussed in Thread: TAS5704 , TAS5760M , TAS5760MD Hi,
Does someone have the reference design for PBTL output with TAS5704 under the condition as below?
PBTL output、Vcc=12V、RL=4Ω、Output Power =20W
or Is it possible to configer the TAS5704…