Part Number: TAS5705 Tool/software: Hi TI Team,
I would like to know what is the frequency response of the Subwoofer PWM outputs. We are planning to use Woofer instead of subwoofer. So, ideally expecting 90–20000 Hz of support.
Kindly provide us…
Part Number: LM49450 Other Parts Discussed in Thread: LM4935 , TAS5102 , TAS5705
Hi,
I am working on a project (Bluetooth stereo speaker) that requires:
2x 2W or 3W speaker
headphones output
Stereo Input (AGC?)
subwoofer output , 20W, with a knob to select…
Other Parts Discussed in Thread: TAS5705 , PCM1851A Dear TI-Support, I am experiencing some trouble initializing my TAS5705: Following the instructions listed on page 44 of the datasheet everything works fine until I reach step 5. Writing 0x00 to register…
Other Parts Discussed in Thread: TAS5705 , TAS5727 After working perfectly for weeks my TAS5705 evm suddenly stopped producing sound.
Simply connecting 3.3v and gnd makes the chip really hot when putting my finger on it. When the problems first began…
Other Parts Discussed in Thread: TAS5705 , TAS5707 , TAS5711 , TAS5717 , TAS5709 Dear Sir,
Is it possible to connect the TAS5707 with external I2S source which don't have MCLK. Base on the datasheet of TAS5705, TAS5707 can generate the internal clock. It…
Other Parts Discussed in Thread: TAS5706 , TAS5705 Hello Texas!
I'm hearing a, however swiftly decaying, white noise when powering up the TAS5706 EVM2 via the !pdn pin. The noise is high freq and sounds like "PFZZzzzz" everytime the !pdn is asserted. The…
Other Parts Discussed in Thread: TAS5705 , PCM2706 I'm using AT89S51 to control TAS5705 through I2C Bus.I want to adjust the volume through I2C interface.(2.0 BTL BD Mode,I2S 16bit 44khz)
Here the steps I've done to initial TAS5705:(MUTE=1,FAULT=1…
Other Parts Discussed in Thread: TAS5705 Hi, Is there a linux driver (or similar driver for a template) for the TAS5705 mated to TI's OMAP3 family of processors? The TAS5705 has an I2C interface for control and I2S interface for data streams. Any information…
Other Parts Discussed in Thread: TAS5705 , TAS5706 TAS5705 and TAS5706 easily provide a (L+R) mono sum to drive an external subwoofer power amplifier, but it is also possible to reconfigure DAP channels to feed the same mono sum to internal power outputs if…