Part Number: TAS5711 Other Parts Discussed in Thread: TAS5705 , Hi team,
Can customer use sine waves as MCLK input signal to the TAS5711 or TAS5705? What's the Vpp Voltage requirements of sine wave? If this is possible to use this way to eliminate EMI…
Other Parts Discussed in Thread: TAS5705 Hi, Is there an available linux driver (or similar driver for a template) for the TAS5705 mated to TI's OMAP3 family of processors? The TAS5705 has an I2C interface for control and I2S interface for data streams…
Hello Ravinder,
Thank you for your reply. I have checked both jumper jp-2 and jp-3 for RCA both are @ADC , all others jumpers included jp-4 is connected pin 1 & 2.
I used a scope probe the line with and without signal for both analog and SPDIF …
Other Parts Discussed in Thread: TAS5705 , TAS5706 , TAS5716 , TAS5760M Hi all,
I2S input power amplifier such as the TAS5705, 06, 16 have sampling frequencies configurable up to 192kHz. However, the maximum audio frequency is not specified.
I would…
Hi, Hanns,
I briefly glanced at the schematics for the TAS5705 EVM and noted that all the pull-ups and downs are on the MC57xx-PSIA board. So, if you wire directly to the TAS5705 board, you might not have the correct pull-up/downs on pins like RESET…
Other Parts Discussed in Thread: TAS5705 Hello!
At a certain stage in prototyping, I wish to connect an external I2S source while still keeping the MC57xxPSIA connector board attached to the TAS5705EVM2 amplifier board.
Would it be possible to remove…
Thanks a bundle, that's really great news. Through a local dealer, I've ordered eval boards for both the TAS5727 and the TAS5705 chips plus some other really nice stuff. Can't wait to it all home and start working with them. I really like D-amps, great…
Other Parts Discussed in Thread: TAS5706B Hi
I have try the setup (2-ch single-end + 1 channel Bridge) for TAS5706B.
However, the 1 channel bridge should be L+R channel.
I have tried the setup based on the "TAS5705-L+R-sum implemetation" but…
Hi,
While I was trying to run the GDE, it said new hardware found by windows, but it could not found the appropriate driver and when I look at the windows device manager I saw a '?' hardware is in my list. I have tried to uninstall and reinstall the…