Other Parts Discussed in Thread: TAS5706 , TAS5602 , TAS5706B Hello,
I'm currently trying to setup the TAS5706 EVM2 with the TAS5602 EVM2 for a 2.1 audio system. After finding the correct values for all my biquad, channel volume, DRCs etc.. using GDE…
Other Parts Discussed in Thread: TAS5706 Hi
I have ordered the TAS5706 Evaluation Module to make the full digital amp..but I can not find the pot to install a attenuator on the board..
Volume can be controlled by software?
Does not the TAS5706 Evaluation M…
Hello again Ravi,
I've tested the configuration changes you suggested and it works well.
I use the down-mix (L+R)/2 mode and take out the bass signal between sub+ and gnd which is then low pass filtered (130Hz cut-off) and then fed to an active subwoofer…
Other Parts Discussed in Thread: TAS5706B , TAS5602 , TAS5706 , TAS5717 Hi all!
What external components are required in order to get a low level signal suitable for a external active subwoofer connected via the subwoofer PWM output of the TAS5706B amplifier?
…
Other Parts Discussed in Thread: TAS5706 , TAS5711 , TAS5717 , TAS5706B Hello all,
I've been spending hours looking at the TAS5706 pwm outputs for headphone and subwoofer through a scope. I can't find anything that looks even remotely like audio in the…
Other Parts Discussed in Thread: TAS5706 , TAS5716 On the TAS5706 and TAS5716, which supply pins (power and ground) are used internally to supply the headphone and subwoofer PWM outputs?
The reason for this question is that we want to include countermeasures…
Other Parts Discussed in Thread: TAS5706A , TAS5706 We have the TAS5706A designed in on one of our class D amplifier products. It's working well, and our customers like it.
Unfortunately, we're running into long lead time issues (~6 months) as we ramp…
Question: I am building an amplifier that is a 2.1 channel configuration. A single stereo input is to be sent to the device and I need a stereo output and a subwoofer. I understand the filtering, but how should I set-up the downmixing?
Other Parts Discussed in Thread: TAS5706 Question: I notice that that the TAS5706 has a PWM output for headphones. Can I drive headphones with it?
Answer: No, the headphone PWM outputs are designed for driving logic. You can use the signals to drive a headphone…
Other Parts Discussed in Thread: TAS5706 The TAS5706 should not create a "pop" when the sample rate is changed; however, some digital audio sources have been observed to rapidly change between the old and new sample rates more than once in a short period…