Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Hi Don,
Thank you for your advice. Just to clarify, that means I can simply use TAS5508/TAS5518 GUI with this board to control those chips?. Do I have to load the firmware to the USB board or can I run directly TAS5508/TAS5518 GUI from the PC to communicate…
Hi, Jorge,
I am not aware of any import restrictions in Argentina. Are you saying that you can't buy an EVM off our eStore?
We don't sell the MC57xx-PSIA as a stand-alone board, but it ships with many of the TAS57xx devices (both TAS5709 and TAS5715…
Other Parts Discussed in Thread: TAS5709 , TAS5707 Dear Sir,
Is there any easy way to set bass boost of TAS5707 just like the TAS5709 bass boost on/off control ?
Is there any example of how the set the EQ of TAS5707 to do bass boost?
Hi Gary,
I can't see your pictures, pleaes click 'Use Rich Formating' to paste the pictures. Please find my answers below:
1. TAS5751M has four bands AGL in processing. So if the power is limited by AGL4, how can I change the volume? I mean…
Hi Don-san,
Thank you for your info.
I understand that TAS5716 support bass boost but not support psycho-acoustic bass enhancement. I will recommend TAS5709 , TAS5710 , and TAS5711 that you recommend in other post.
Best Regards,
Sonoki
Hi, Evgeny,
TAS5709, TAS5710, and TAS5711 all have MUCH better surround effects than the '5716.
Unfortunately, none of these support 192 kHz, so if that's a hard requirement, you will have to stick to the older parts. We dropped 192 kHz support on…
Other Parts Discussed in Thread: TAS5705 , TAS5707 , TAS5711 , TAS5717 , TAS5709 Dear Sir,
Is it possible to connect the TAS5707 with external I2S source which don't have MCLK. Base on the datasheet of TAS5705, TAS5707 can generate the internal clock. It…
Other Parts Discussed in Thread: TAS5709 , TAS5719 , TAS5719EVM , TAS5717EVM Hello,
I have downloaded TAS570X GED (2.1 build 14). When i start a new design, on the right side, i can select the device. My problem is that only 5707, 5708 or 5709 appear? If…
I have now tested the unit with 6 boards (12 channels) connected in parallel and the I2C part seems to work fine!
I can send the same messages to all six TAS5709's at the same time!
There have been two problems though, that I would like to mention…