Other Parts Discussed in Thread: TAS5715 , TAS5717 , TAS5716 , TAS5706B I'm currently considering using the TAS5715 for a new design but I'm a bit confused as to what the data sheet states regarding line out.
It states
The TAS5715 provides headphone…
Other Parts Discussed in Thread: TAS5715 I am using the TAS5715 in a single speaker application and need to drive a tweeter and woofer using the two pairs by implementing a high and low-pass filter, one on each output. The datasheet seems lacking in how…
Other Parts Discussed in Thread: TAS5715 , TAS5715EVM Hello!
I have made a board with the TAS5715. The board is based on the TAS5715EVM. My board has a much higher current consumtion without any load. I figured out, that a part of the output filter is the…
Other Parts Discussed in Thread: TAS5715 Hi,
I'm looking far a version S/W I can use to program the TAS5715. I have the S/W from the TAS5715 page for the EVM but it doesn't allow me to program the DRC's and other parameters, or allow any change to…
Other Parts Discussed in Thread: TAS5715 , TAS5713 Hi,
I have been looking at the TAS5713 and comparing it to the TAS5715. In terms of output power they seem very similar. Are there any output power advantages to using the TAS5715?
Thank you
Other Parts Discussed in Thread: TAS5715 Hello guys, We are planning to use a TAS5715 I2S-Audio-Amplifier, but we need an output power of at least 40W per channel. Please let us know if the following way would lead us to success: The source is a VS1053 (MP3…
Other Parts Discussed in Thread: TAS5715EVM , TAS5715 , DIR9001 I am attempting to get a TAS5715EVM up and running to do an evaluation of this amplifier, but the behavior I'm seeing doesn't make a lot of sense, and the documentation is not entirely clear…
Part Number: TAS5715EVM Other Parts Discussed in Thread: TAS5715
Dear TI team member,
We are using the TASS5715EVM to adjust the EQ for a subwoofer speaker. Hope it can filter the high pitch out , and only show the bass effect (30Hz--240Hz).
When we adjust…
yes we did follow the procedure in the attached document.
Please make sure the environment variables is "54" as you guide in the attached document for TAS5715 .
Is that a possible because the environment variables should not be "54" ?…