Other Parts Discussed in Thread: TAS5717 Hello,
We are using the TAS5717 in our design and we need to program the biquad filters. I have generated a set of coefficients in Matlab, but when I activate the biquad on the Amp, I only get a very high pitch…
Other Parts Discussed in Thread: TAS5717 The customer has got a question about TAS5717. See below:
I have question if it is possible to send audio data with format different than in specification. In our case data transfer looks like on drawing below…
Other Parts Discussed in Thread: TAS5717 I am trying to communicate with a TAS5717 using I2C without any luck. The +3.3v supply seems to be correct and another device (EEPROM) on the same I2C bus is working ok.
The reset and power down pins are both high…
Other Parts Discussed in Thread: TAS5717 Hello, I would like to know on the outputs of the TAS5717 OUTA,B,C,D, is there a problem with tying the designated minus outputs say B and C together for a common connection? We have a situation where, like a headphone…
Other Parts Discussed in Thread: TAS5717
Hi,
In my project, I intend to use a C5000 MCU to interface with TAS5717
via the I2S protocol. The MCU is the master, and TAS5717 is the slave.
For the I2S protocol, TAS5717 has 4 pins:
- LRCLK
- SCLK
…
Other Parts Discussed in Thread: TAS5717EVM Hi,
Some one have TAS5717EVM User Guide for application?
I can't find it on the web.
I need to know BOM parts & surrounding parts conexion. Thanks in advance
RCP
Hi Ian,
Seems your I2C can work normally and TAS5707 has acknowledge. But TAS5707 and TAS5717 have obvious DAP PROCESS STRUCTURE so that you cannot use TAS571X code to initialize TAS5707. Suggest you to apply for one TAS5707 EVM and GDE software to…
Other Parts Discussed in Thread: TAS5717 , TAS5717EVM , TAS5713 , TAS5727EVM Hello,
I've no so much experience about how translate Q,Fo,Filter type & Gain from Main micro to in order to control TAS5717 PEQ parameters.
Usually, by using main micro…
Hello Matthew,
DVDD/AVDD is necessary for device operation. You can look at TAS5717/19EVM User's Guide for a schematic showing the components we recommend for proper device operation. If you don't need to test a working output you can disconnect the…