Part Number: TAS5717 We draw the circuit diagram according to the reference design of TAS5717EVM, but we found that the voice of speaker is normal, and the voice of headphones is very low.
The headphones is I2S input and we set 0x05 register is 0x13 when…
Part Number: TAS5717 Hi Team,
Would you share your mailing list for sending email because I'd like to ask questions with my confidential information ?
Thanks
Part Number: TAS5717 Other Parts Discussed in Thread: TAS5806MD Is it safe to run this chip with a light or no load? Specifically, I have a product in which the TAS5717 is used to drive two small 8-ohm speakers. The output has an LC network which I have…
Part Number: TAS5717 Hi Sirs, According to TAS5717 datasheet, there is an internal 15kR pulldown to GND with the A_SEL pin. Does the internal pull down resistor take effect with headphone driver enabled? If we don't use headphones driver (0x05 = 0x00)…
Part Number: TAS5717
Hi Team, Customer uses TAS5717 and sometimes it will do not has the sound output. (the fail situation can be duplicate once in 100times. fail rate 1%) The I2S is from audio codec. The audio codec won't send the I2S all the times.…
Part Number: TAS5717 My customer is having a couple of issues with a custom board using the TAS5717:
1. With any I2S traffic, even with a silent audio, the output will oscillate at 8Hz. Tones will play on top of this low frequency and sound okay.
2. Any…
Part Number: TAS5717 Hi Sirs, Would you pls provide TAS5717's official efficiency data with 4ohm load and 12V, 20V PVDD each per customer's request? We saw 8ohm's efficiency chart on the datasheet only.
We assume the 4ohm's efficiency could…