Part Number: TAS5717 Hi Sirs, Would you pls assist me to review of my proposal for TAS5717 BD modulation for BTL and PBTL modes? BTL (stereo):
------------------------------------------
#Enable PLL
0x1B = 0x00
# BD Modulation
0x20 = 0x00 89 77 72
0x11…
Part Number: TAS5717 Hi Sirs, Is there any internal power limit in default with TAS5717? I found the TAS5717 EVM sends up to 1.2W, 4ohm load, 1% THD+N with 5VPVCC. Would you pls advise that can we achieve 2W, 4ohm, <1% THD+N with 5VPVCC? I send the following…
Hi Petr,
Very glad to know your SW is working as expected now. Unfortunately there is no way to write the coefficients at the same time on TAS5717, because this is an old device. So when changing the BQ efficients on TAS5717, need to mute the output signal…
Part Number: TAS5717 Hi,
I use software GDE to config TAS5717 as well, But I think TAS5717 once turn off the device, all of config will be clear, is it right?
It means TAS5717 data is stored in volatile memory,is it right?
I want to software download…
Part Number: TAS5717 Other Parts Discussed in Thread: TAS5760MD HI, everyone.
I need information about TAS5717.
If I finish software coding using GDE to download TAS5717 then TAS5717 always need MCU for I2C commucation ?
TAS5717 does not have memory…
Part Number: TAS5717 Other Parts Discussed in Thread: TAS5753MD
Hello I need to design a system with digital I2S input + 3W (or above) stereo amp, with a TAS5717 at 1.65$ is there a cheaper solution out there?
My constraint is a power supply of 5v …
Part Number: TAS5717 1 I use TAS5717 THD+N=1%,.12V power supply, 6 ohm speaker, now that the speaker output voltage is only 3.1V, I want to make the 8W sound, when the output voltage increases, there is the distortion of the situation, how do I do now…
Part Number: TAS5717 Other Parts Discussed in Thread: TAS5721 , TAS5731M , TAS5719 Hi Team,
The customer would like to use TAS5717 for the single ended output.
Would you provide a reference schematic for the single ended output? How to modify the registers…
Part Number: TAS5717
Hi Team, Customer would like to use TAS5717 on the new project.
Could you help for the following two questions? 1. If customer set PDN to low and back to high, will all the I2C be back to the default values? Or TAS5717 will keep the…