Part Number: TAS5717
Hi Team,
The customer is using TAS5717. There is not any noise when the customer uses the speaker to output. But there is much noise when the customer uses the
headphone to output. Even if the customer change another headphone, there…
Part Number: TAS5717 Hi Sirs, The TAS5717 datasheet provides recommended ICD configurations for AD and BD modulation schemes: However, we fonnd different configuratin on the TAS5717 EVM's GUI, captured by I2C analyzer: AD modulation:
0x11 = 0xB8
0x12…
Part Number: TAS5717 Hi Shawn,
Customer would like to see the performance graph, THD+N vs Frequency
Output 20W into 4ohm load in PBTL mode.
The graph in datasheet is based on 8ohm in BTL mode.
Could you help to provide it?
Thank you.
Sincerely,
Will…
Part Number: TAS5717 Hello.
Our project used TAS5717 output for 2W 4 Ohm speaker got noise but 8 Ohm speaker is OK.
TAS5717 Master Volume setting to 0 dB at 1kHz input. NB volume set below 67 Speaker output waveform is OK.
NB Volume set above 68 Speaker output…
Part Number: TAS5717 Hi folks,
Do we have Output Power vs THD+N graph of TAS5717/9 in PBTL mode?
The impedance of load is 4ohm.
Do you have TSA5717/9 reference schematic in PBTL mode?
Thank you.
Sincerely,
Will Liu
Part Number: TAS5717 Hi :
We use the TAS5717 as the Audio DSP & AMP, and there has the noise (sound like the current noise, fix frequency), the earphone and speaker both have.
The attachment is the schematic and register map, pls take a review them…
Part Number: TAS5717
Hi :
We use the TAS5717 as the Audio DSP & AMP, and there has the noise (sound like the current noise, fix frequency), the earphone and speaker both have.
The attachment is the schematic and register map, pls take a review them…
Part Number: TAS5717 Hi Team,
Can TAS5717 use external oscillator to provide the MCLK without syc the BCLK and LRCLK?
it means the BCLK, WCLK and Data is from scalar. And scalar do not sync the clock with the osicillator.
Is that MCLK need to sync with…
Part Number: TAS5717EVM Other Parts Discussed in Thread: TAS5717 HI, everyone.
I need information about TAS5717.
If I finish software coding using GDE to download TAS5717 then TAS5717 always need MCU for I2C commucation ?
TAS5717 does not have memory…