Part Number: TAS5719 Other Parts Discussed in Thread: TAS5717 Is there a diagram or list of the minimum number of connections and external parts necessary to get the TAS5719 up and running in order to access the I2C bus without any of the I2S or any of…
Part Number: TAS5719 I want to know about the TI TAS5719's pressure function. And I found that debugging DEMO boards, sometimes the output amplitude will be different! For example, the first time I turn on, I can output the level of about 4V, but I only…
Part Number: TAS5719 Other Parts Discussed in Thread: TAS5713 , TAS5733 Hi team,
After tuning the EQ of TAS5719 in my customer system, they would like to write the data into the device in their production. Would like to verfiy the sequence and what register…
Part Number: TAS5719EVM Other Parts Discussed in Thread: TAS5719 Dear,
One customer used TAS5719EM to test the SNR, he tested the output noise floor of headphone higher than 110uV, SNR is 83dB.
The test condition is as this:
1. Connected external 12V regulator…
Part Number: TAS5719 Hello, our customer is facing following issue at new product design.
(1) As the datasheet said,
BKND_ERR REGISTER (0x1C) When a back-end error signal is received from the internal power stage, the power stage is reset, stopping al…
Part Number: TAS5719 Hello,
Our customer wants to refer TAS5719EVM pattern layout.
We can find PCB drawing in EVM manual however it is difficult to see a detail.
How can we get gaver file?
Regards,
Mochizuki
Part Number: TAS5719 Other Parts Discussed in Thread: TAS5717 , Hi Sirs, The TAS5717/TAS5719's MCLk and BCLK input must be aligned with each other as we know. Would you pls advise if we can make them align on falling edge as the picture below? Thank you…
Part Number: TAS5719 Hi Team, My customer uses TAS5719. We try to write 0x00 into register 0x1B and we found the readback value from register 0x1B is 0x0C0. Is that expected result?
Thanks, SHH
Part Number: TAS5719 Hello team,
The customer had a question about Short Protection at HP_PWML/R pins.
I do not believe that TAS5719 has over current protection function, however TAS5719 does not break even if HP_PWML/R pins connected to GND (short condition…
Part Number: TAS5719
Hi Team, My customer would like to evaluate TAS5719 for the 3 wire I2S. IF not connecting MCLK, will the amp still work? What is the concern if not conneting MCLK?
Thanks, SHH