Other Parts Discussed in Thread: TAS5717 , TAS5731 , TAS5713 , TAS5719 , TAS5731M Hi,
We believe that the power on/off sequence which you recommend for TAS5717 and TAS5719 is same with TAS5713 and TAS5731.
Is our understanding correct ?
Best regards,
…
Other Parts Discussed in Thread: TAS5717 Hi,
Could you please tell us the recovery time from the overcurrent protection if a short circuit on the output is removed ? Moreover, when is /FAULT pin asserted to low although the overcurrent response time is…
Other Parts Discussed in Thread: TAS5719 Dear Sir,
We have a problem when using TAS5719 .
When power on and send reset / PND and I2C command. Speaker is no output.
If we short PDN to GND and release it to 3.3V. Output is OK!
Can you give me a suggestion…
Hello Mark,
Please review the attached presentation on TAS57xx audio processing blocks. Let me know if it answers your questions or you have additional questions.
7268.TAS57xx DAP Training 2014.pptx
Other Parts Discussed in Thread: TAS5719 , AM3517 Hi,
We're developing a TAS5719 driver for the linux 2.6.37 kernel from the am3517-evm-sdk-05.05.01.00. Our custom board has a
AM3517 sitara. The TAS5719 is a slave I2S device connected to the Sitara…
Other Parts Discussed in Thread: AM3517 , TAS5719 Hi,
I still have problems with my AM3517 board with the TAS5719 codec. Now I have the SCLK and MCLK tied together but only work when
the MCLK frequency is in range (from datasheet this is from 2.8224 to…
Other Parts Discussed in Thread: TAS5719 , TAS5719EVM Hi,
I can not get the TAS5719 to communicate with the MC57xxPSIA. VR_DIG and VR_ANA have 1.8 V on them so we think the chip is powered on. A_SEL is high, like the EVM, so the I2C address should be 0x56…
Other Parts Discussed in Thread: TAS5709 , TAS5719 , TAS5719EVM , TAS5717EVM Hello,
I have downloaded TAS570X GED (2.1 build 14). When i start a new design, on the right side, i can select the device. My problem is that only 5707, 5708 or 5709 appear? If…
Part Number: TAS5751M Other Parts Discussed in Thread: TAS5719 , TAS5805 Hello,
Our customer try to utilize TAS5751M with x6 AAA battery. PVdd range would be 9.0V to 5.4V.
When look at the data sheet recommended operation condition PVdd mini is 8.0V. And…
Other Parts Discussed in Thread: TAS5719 Does this device (TAS5719)support other sample rate not defined in the "clock control register"
if i want to use fs = 31KHz, which value should i write to the clock control register.