Part Number: TAS5720A-Q1 Other Parts Discussed in Thread: TAS6511-Q1 Tool/software: Hi,
I would like to use the TAS5720A-Q1 for an AVAS (Acoustic Vehicle Alert System) but I need the speaker diagnostic feature (open, short...).
Can you tell me if…
Part Number: TAS5720A-Q1 Tool/software:
Hi Team,
We have designed an audio amplifier using the TAS5720A-Q1 and verified the design in hardware configuration mode with the TAS5720A-Q1 EVK. Currently, our custom board is in the bring-up stage and…
Part Number: TAS5720A-Q1 Tool/software: Dear TI experts,
1. Can I know the way to calculate each current consumption of AVDD and PVDD depends on the spec. of speaker?
(i.e. current consumption of PVDD and AVDD if my customer use 25W speaker)
2.…
Part Number: TAS5720A-Q1 Other Parts Discussed in Thread: CC2642R-Q1 Tool/software: Hi Team,
I see CC2642 support I2S and TAS5720 also has mono I2S port.
And I would like to check if TAS5720-Q1 can pair with CC2642R-Q1 or not?
Regards
Roy
Part Number: TAS5720A-Q1 Hello,
I am working with TAS5720A-Q1. At the power up, I set the following registers :
REG ADDRESS
DATA
0x02
0x04
0x01
0xFD
0x06
0xD1
The others are kept as default.
The master and…
Part Number: TAS5720A-Q1 Hello,
We are using TAS5720A for audio application. We are able to configure the device using I2C in software mode and able to generate the sounds but we see a weird behavior during start of the sound.
The issue is some portion…
Part Number: PUREPATH-CMBEVM Other Parts Discussed in Thread: TAS5720A-Q1 , TAS5720A-Q1EVM Dear TI team and community,
we already managed to connect the TAS5720A-Q1EVM to the PUREPATH-CMBEVM and got it working on PurePath Console 1. Now we have designed…
Part Number: TAS5720A-Q1 Other Parts Discussed in Thread: TAS2780 , , TAS6421-Q1 , TAS6424-Q1 , TAS6584-Q1 , TAS6424E-Q1 Tool/software: Hello TI Audio Support Team,
I've been evaluating the TAS2780 and really like the digital aspects of the amplifier…
Part Number: TAS5720A-Q1 Tool/software: Hi Gregg,
In our design, LRCK is not generated always. It is generated only when there is a valid audio request from application. Other clocks SCLK and MCLK are generated continuously.
In order to remove…
Part Number: TAS5720A-Q1 Hi All,
i am interfacing TAS5720A-Q1 ( software control ) with my controller.
could you please explain me these pins of TAS5720A-Q1.
purpose / Configuration (Timer for Digital IO)
LRCK
SDIN
MCLK
SCLK
I2C (SDA …