Part Number: TAS5720L Currently using mcu`s clock output is fixed and as below, When WS is 43.71kHz, CK = 1.4MHz and MCK = 1.4MHz
But when WS is 86kHz, CK = 2.8MHz and MCK = 2.8MHz.
So as accepted clke pin indicate clock error and nothing comes out…
Part Number: TAS5720L Hi,
Our customer is using TAS5720L device.
The issue is that output p/n is common not differential.
Could you please check and guide?
* Register setting
[0x00]Audio Device ID = 0x01 [0x01]Audio Power Control = 0xFD [0x02…
Part Number: TAS5720L Hi,
I am fairly new to designing audio hardware. This post is to just reassure that my understanding is correct. Initially I was confused regarding what my ideal PVDD value should be.
We are planning to use the following speaker…
Part Number: TAS5720L Other Parts Discussed in Thread: TAS3251 Hi
We are working on a project with TAS5720.
We use mediatech MCU to send i2s to TAS5720.
Below is our design diagram. Please note we have had 1 design for this IC series and it…
Hi Matthias,
Was the /FAULTZ pin ever pulled low?
If a SAIF clock error occurs, TAS5720L will go into the sleep mode and the /FAULTZ pin becomes low.
Andy
Part Number: TAS5720L Other Parts Discussed in Thread: TAS5782M , TAS5754M Hi,
I am using TAS5720L on my new project. It only has a mono speaker output and driven by TAS5720L. I can set either L or R audio channel output from the speaker by different…
Hello customer,
As to TAS5720L, LC filter is recommended for reasons below:
EMC: this is a mono device, EMC is hard to pass if no LC is used even on your condition;
Performance:
Efficiency & thermal: LC help to improve the efficiency compared…
Part Number: TAS5720L Hi Sirs, Would you please advise the TAS5720L's DVDD and AVDD power consumption for customer's design reference? Thank you and Best regards, Wayne Chen 03/02/2018